Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulation of sheet metal assembly with localized loading.

Experimenter
Experimenter

Hi All,

I am trying to simulate a static loading on a sheet metal surafce. The load is localised on a square area of the surface and the surface is supported by 3 supports as the picture below shows.

 I am familiar with surface split for sheet metal part but not assemblies. any idea how to approach this problem.?

 thank you

 

pic2.PNG

 

pic1.PNG

6 REPLIES

Re: Simulation of sheet metal assembly with localized loading.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is this for use with Simulation Express?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Simulation of sheet metal assembly with localized loading.

Experimenter
Experimenter

No... this is for the full simulation licence.

 

 

Re: Simulation of sheet metal assembly with localized loading.

Experimenter
Experimenter

just for clarification i am using Solid Edge 6ST

Re: Simulation of sheet metal assembly with localized loading.

Siemens Phenom Siemens Phenom
Siemens Phenom

Abdel,

maybe have a look at the Help Activity:

"Apply a mixed mesh to an assembly". 

Or consult with your local reseller/support.

 

This was my quick test in ST7.

Solid Edge ST7 - Simulation Results - [Asm1.png

/Ulf Eriksson

Siemens EMEA GTAC Support

Re: Simulation of sheet metal assembly with localized loading.

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Maybe I am missing something, but why don't you just go into the sheetmetal part and split the surface?  Then you have some geometry in the assembly to apply the load to.

Re: Simulation of sheet metal assembly with localized loading.

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, you can do it!

 

The important step is that sketch has to lie on the mid-plane!

 

Here is a video about steps. This video is divided two parts, in the first I'm using simulation geometry and in the second I'm using part to FEA model.

 

 

BR,

Imics
http://solidedgest.wordpress.com/