Cancel
Showing results for 
Search instead for 
Did you mean: 

Sketch Library

Valued Contributor
Valued Contributor

New to SE. Are there sketch libraries like hex, I beam, star, etc? I am using ST7 for training, but may use ST5 for client?

3 REPLIES

Re: Sketch Library

Gears Phenom Gears Phenom
Gears Phenom

Solid Edge in my knowledge does not come with standard shapes for sketching though it is easy to create a library. Here's how:

 

 

This feature is available in both ST5 and ST7 though the library created in ST7 cannot be used in ST5.

 

~Tushar Suradkar

www.SurfAndCode.in

 

Re: Sketch Library

Valued Contributor
Valued Contributor

Nice Tushar! Your site is very happening as well. Thanks so much!

 

Is there a way to aquire standars sketch libraries that date back to at least ST5?

 

 

Re: Sketch Library

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So is it true that these features are dependent on their sync/ordered creation mode? IOW, a feature created in ordered only works in ordered and a sync feature only works in sync.

That's my experimental experience.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200