Cancel
Showing results for 
Search instead for 
Did you mean: 

Sketch dimension don't zoom when zooming in/out

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

I'm experiencing something strange since last friday, when in sketch i place dimensions but if i zoom in or out of the geometry the dimensions follow the geometry which turns the dimension too small.

 

Anyone experienced something like this? Probably something i've touched unintentionally.

 

Thank you!

3 REPLIES 3

Re: Sketch dimension don't zoom when zooming in/out

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try these switches:

 

PMI dims.JPG

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Sketch dimension don't zoom when zooming in/out

Experimenter
Experimenter

Hello,

 

Refer attached Image.

Highlighted

Re: Sketch dimension don't zoom when zooming in/out

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Sn 

 

 

 

this is the Solid Edge forum rather than the NX forum.

So the form looks more like coming from NX than from SE, isn't it?

 

 

regards
Wolfgang