Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Sketch paste rotation?

Valued Contributor
Valued Contributor

I extracted the sketch from another Part
Ctrl + C
Ctrl + V to add another document.

I want to attach it to the desired position .. Can not I rotate the sketch in the ideal state?
Just as you can rotate a block when you load it ....
When I paste the extracted sketch, I think I can not rotate it.
Is it possible?

 

skech1.pngsketch2.png

I want to rotate when pasted with Ctrl + V
I want to rotate a block like a simple keyboard key ...

2 REPLIES 2

Re: Sketch paste rotation?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Hclee,

 

No, not in the context of the "Paste" function....but while it is highlighted [pre-selected], you have all of the standard Sketch tools available to you, in order to Rotate, Scale, etc....also Relate / Dimension to obtain the  result you desire.  HTH.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Sketch paste rotation?

Valued Contributor
Valued Contributor

hmm

Thank you for answer...

 

hope this feature ...