Cancel
Showing results for 
Search instead for 
Did you mean: 

Sketch

Creator
Creator

Hi,

 

I am new to solidedge.

When I sketch Rectangle or circle in sketch and gave dimension to them

They don t have any constrain like perpendicular or Dimension which I gave.

See Attach photo.

2 REPLIES

Betreff: Sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Raumik

 

 

 

this seems to be one of the standard issue when beginning with SE

 

There are 2 settings You have to take care

 

One is that the "Keep Relations" button must be ON

This is the marked button in the top line of the tab

 

 

 

 

 

20170305_1912.PNG

 

The other is, that the dimension itself must be declared as DRIVE and not driven

This is, the lock sign in the dim tab must be on.

 

You see, that a dimension is at DRIVE that it is shown in red where a driven dimension normally is blue.

 

The default values for those settings normally are as mentioned but somehow You or another user might changed it.

 

Set it back and draw Your rectangle again, give the dimensions to it and YOu will see, everytihng works as expected

 

 

 

regards
Wolfgang

Betreff: Sketch

Creator
Creator
Thanks...