Cancel
Showing results for 
Search instead for 
Did you mean: 

Slanted assembly in coordinate system

Pioneer
Pioneer

Hi all

Nice day?...^^

 

Please see the picture below.

112333333.png

The parts that make up the assembly in the coordinate system are tilted as shown.

 

This is seen from the front as follows.

2233.png

I do not know the angle.
You have to adjust to the decimal place
It becomes troublesome.

 

44433.png

I would like the parts to look straight using the steering wheel.
I do not know how good.

If someone knows a good way, please let me know.

 

I want to look at the picture.

1199.png

 

file Attch

 

 

 

 

5 REPLIES 5

Re: Slanted assembly in coordinate system

Gears Phenom Gears Phenom
Gears Phenom

since this is an assy.   i would suggest using the mate or planar aline relationship to align the faces.

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Slanted assembly in coordinate system

Pioneer
Pioneer

Oh right.
I did not think that it was a combination of Ass and Transfer.
Ground conditions were unpacked and assembled .. ^^
Thank you.

Betreff: Slanted assembly in coordinate system

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee1

 

 

just go to the Occurancey Properties and change the values for the basic part!

 

20180426_1535.pngbefore modification20180426_1537.pngafter modification

regards
Wolfgang

Betreff: Slanted assembly in coordinate system

Pioneer
Pioneer

Thank you. hawcad


Here is another question !!

Is it an often used feature?
When do you use it often?

Sorry for the many questions .. ^^

Betreff: Slanted assembly in coordinate system

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee1

 

 

Yes, of couse.

I use that function often, not to say very often.

 

First, if the base part of an assembly is not modelled in the wanted orientation or position, I use the x, y, z position and rotation to fix it.

 

And further, I have to define those additional props, like "show in higher level", "is reference", "show in draft"  and so on for certain components.

 

From ST9 on, You also can add Custom Occurency Properties, which I use too.

 

 

 

regards
Wolfgang