Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Slot - multiple copy in context

Pioneer
Pioneer

Hello

 

I've two parts. ( P1)  where is a lot  of holes. All holes are placed irregulary.

P2 - in this part I want to place slots.

Both parts are placed in one assembly ( parts are connected with face)

I want to place slots in P2. But middle of slot must be connected with middle of hole of P1.

I made it it in context. But I've problem because I can not to place multiple slots in one operation.

For "slot" tool it's possible to draw only one skech. I want to be placed onoe slot on each hole.

So - If I can't place multiple sketch in one operation of slot I have to copy each operation of slot for all holes

How to do this  faster?

 

Regards

 

Marcin

 

 

 

 

3 REPLIES 3

Re: Slot - multiple copy in context

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@SUCHY wrote:

How to do this  faster?


Copy-Pasting the Slot feature to the Feature Library is one way I can think to make it faster.

Right-click on the Slot feature in the graphics or the PathFinder and Paste in an empty space in the Feature Library. Then drag back the slot library feature into the part.

Re: Slot - multiple copy in context

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


one way would be the table pattern of ST8

 

You have one exel table with the origin positions of holes and slots and You can use it for both parts

So both pattern always will keep equal

 

regards
Wolfgang

Re: Slot - multiple copy in context

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

@hawcad's & @Tushar's solutions are good. It depends on many things (number of holes, modeling environment, modeling method, SE version...)

 

Here is a video about some solutions (synchronous copy, duplicate, pattern...)

 

BR,

Imics
http://solidedgest.wordpress.com/