Cancel
Showing results for 
Search instead for 
Did you mean: 

Slow Start up of st9 on windows 10

Creator
Creator

I just got a new laptop with Win 10 ver. 1803. On my old win 7 machine ST9 MP14 would take about 10-15 secs to start up but on the new machine it takes a minute and a half. Works fine after that. Any ideas? 

4 REPLIES 4
Highlighted

Betreff: Slow Start up of st9 on windows 10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Bert303

 

 

 

could this be come from any antivirus/security etc. scan?

 

 

regards
Wolfgang

Betreff: Slow Start up of st9 on windows 10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Bert303  Hard to say between 2 different PC's...

 

  • Hard drive differences - was the old one a fast drive like SSD or 15000RPM SCSI and the new one a 7200RPM SATA?
  • As @hawcad mentioned, virus scanner turned on and scanning the application on the new and no virus scanner on the old or there was an exception for Solid Edge.

I'm running 1803 and SE only takes about 9 to 10 seconds to start but I am running a fast SSD.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Slow Start up of st9 on windows 10

Creator
Creator

Thanks guys, I'll check into the virus protection with my IT guys. 

The old hard drive was a Western Dig 7200 rpm SATA (WD5000AAKX-083CA1), nothing special really. The new one is a samsung ssd (mzvlw256hehp-000L7), again nothing special by todays standard but I'd expect it to be faster than the 4 year old one. 

Betreff: Slow Start up of st9 on windows 10

Creator
Creator

Yep, Kaspersky's the culprit. 

Thanks again.