Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Slow performance ST10 at new workstation HP Z6 G4

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Thanks for the info @uk_dave.

When I return to work I will evaluate it.

Regards.

Re: Slow performance ST10 at new workstation HP Z6 G4

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad  We are currently using the HP 15.6" ZBook 15 G4 Mobile Workstation

 

Performance

ProcessorIntel Core i7-7820HQ Quad-Core
Base Clock Speed2.9 GHz
Max Boost Speed3.9 GHz
Total Installed Memory16 GB
Maximum Memory Capacity64 GB
Memory TypeDDR4 SDRAM
Memory Speed2400 MHz
User-Replaceable Memory1 x 16 GB
Available Memory Slots3
Memory Slot Type260-Pin SO-DIMM
ECC MemoryNo
Graphics TypeDedicated
Graphics CardNVIDIA Quadro M2200 with 4 GB GDDR5 VRAM


Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Slow performance ST10 at new workstation HP Z6 G4

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

 

thanks for that info, sounds great.

 

I believe that with a notebook there are less problems than with workstations, where many configurations, dirvers, etc. are in use.

 

 

regards
Wolfgang

Re: Slow performance ST10 at new workstation HP Z6 G4

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcadPossibly the mobile workstations are better "engineered" since you don't have as much variability in the component selection.  We don't buy too many desktops anymore as everyone needs to be mobile, but we also buy the Z240 mini towers for those who need/want them and they are also working fine.  Similar specs...



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Slow performance ST10 at new workstation HP Z6 G4

Experimenter
Experimenter

I think adding more RAM would help and also update the drivers for the graphics card.

https://graphicscardhub.com

Re: Slow performance ST10 at new workstation HP Z6 G4

Experimenter
Experimenter

Hi hawcad,

 

I also use Hp Zbook and not have problem with Solid Edge ST10 performance. 10000+ difficult part and assembly.

My config:

I7 4800HQ 3,7 GHz

8GB ram

256 SSD

Quadro k2100M 2GB

 

Comment: when work with Solid Edge I sett manual my laptop max performance.

 

Regards,

Tibor