Cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Dimensions

Pioneer
Pioneer

Can you change format values in smart dimensions like you can in callout properties?

 

For example I want a hole dia to be .xxx but the the depth only needs to be .xx

1 REPLY

Betreff: Smart Dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @lostriver319

 

 

I think You have to use format styles therefore!

 

Create them so You can use them per easy selection in 3D 

 

 

 

If You are talking about drafts, then I would prefer the dimension type as selection method.

Use "feature legend" for holes where You clearly can define how they should look like.

And in options - dimensions  You can define which type should use which format style.

 

I will try to make some pictures when back in the office with a SE computer running

 

 

 

regards
Wolfgang