Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Smart Quantities

Valued Contributor
Valued Contributor

I'm having trouble showing smart quantities in my callouts.  Is there something I'm missing?

 

Also, is there by any chance a way to replace the symbols with text (to keep with my company's format)?

 

Thanks in advance,

 

Matt

 

3.JPG

 

4 REPLIES 4

Re: Smart Quantities

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Matt,

Did you add %QN to the hole types on the Feature Callout tab?

If you ever see it report 0 try Ctrl+Shift+Update Views command.

LMGi
www.TLMGi.com

Re: Smart Quantities

Valued Contributor
Valued Contributor

No Jason, I did not.  Not quite sure how the Smart Depth and Feature Callout tabs interact with each other.  I guess I thought that since the "thru" suffix came automatically from the Smart Depth tab, the Quanitity callout would also be there.

 

I've always just used multiple custom callouts for different features to get the formatting that I wanted, but would like to start just using the %HC all the time.  I have some more reading and experimenting to do.

 

Thanks,

 

Matt

Re: Smart Quantities

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

%HC means go determine the hole type on the Feature Callout tab.

Then if you use %ZH or %ZT or %QN in any of the hole type fields it will continue to the Smart Depth tab.

 

If the quantity of the holes returned is 1 from that tab then it will ignore everything in the field for quantity like "X" or "PL" etc... Thats cool (smart).

 

But if you use "%QA X" directly in the hole type field on the Feature Callout Tab you get 1 X even if there is just one hole.

 

LMGi
www.TLMGi.com

Re: Smart Quantities

Valued Contributor
Valued Contributor

Got it.  Thanks Jason.  The Counterbore area in Feature Callout tab was missing info. and confusing me.

 

Thanks again.