Cancel
Showing results for 
Search instead for 
Did you mean: 

SmartDimension button

Not applicable

Dear Friends,
As a new user of the 2D Solid Edge I´m facing some problems to visualise the SmartDimension
button in my vertical toolbar. I made a permmited free down load from the official
website. Is this a complete version or a demo one? I run XP professional with 728
MB RAM. Is it enough to manage the software?
Any help will be really appreciated.
Many thaks,
Octavio
1 REPLY 1

Re: SmartDimension button

Not applicable
Octavio,
If you have just now installed the software, you should see the
SmartDimension command just below the Detail View command. Is the
SmartDimension command button the only one missing? Do you see the Distance
Between dimension command?
Regards,
Rick B.