Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge 2019 MP7: Draw Explode Lines?

Good afternoon everyone,

 

After installing MP7 it seems that the "Draw" explode lines function is broken. When manually drawing the explode line, the line is created between the original design position of the parts and not the exploded positions of the parts.

 

Can someone please see if they can reproduce this error?

 

Capture.JPG

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3
3 REPLIES 3

Re: Solid Edge 2019 MP7: Draw Explode Lines?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@TheodoreTurner I can confirm the issue.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge 2019 MP7: Draw Explode Lines?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Problem Report has been logged. Have asked this be fixed in MP8. 

Re: Solid Edge 2019 MP7: Draw Explode Lines?

Thank you @andersj 

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3