Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge 2019 - Maintenance Pack 6 Announcement

Siemens Legend Siemens Legend
Siemens Legend

April 13, 2019

 

Dear Solid Edge Customer:

 

Solid Edge 2019 Maintenance Pack 6 is now available for download.

 

Sincerely,

The Solid Edge Team

 

============

Release Notes:

============

 

Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

 

Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.

 

=====================

Maintenance Pack Version:

=====================

 

Solid Edge 2019 MP6

Version: 219.00.06.04

 

================

Download Location:

================

 

Solid Edge 2019 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/

 

==========

Installation:

==========

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
  • MSI Product Updates calculate free disk space before installing. Please be patient.
  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
  • Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
  • When uninstalling, the original source media must be available to allow the recovery of previous file versions.
  • The current MSI Product Update will be the only Update listed and available for uninstallation.
  • After the current Product Update is uninstalled the previous Product Update will become the current Update.
  • .zip files delivered with this MP such as SEECAdministratorV219.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

 

For details on initiating your email subscription navigate to:

https://www.plm.automation.siemens.com/global/en/support/email-subscription.html

 

============================================

This Maintenance Pack addresses the following PRs:

============================================

 

===General===

PR 9261665: Engineering reference, Gear design update problem

PR 9280124: Lower graphic card performance on "Tools" ribbon

PR 9311226: Poor performance when checking out a floating license with options

 

===API===

PR 9398903: Parts being placed in the wrong position during reorder

 

===Assembly===

PR 9350209: Solid Edge is crashing while running route by part command

PR 9363289: Failed to extend/trim the highlighted frame component(s) using the selected tool

PR 9391936: Flickering when zooming in sketch edit in place in assembly

PR 9376223: Assembly File repair SE2019 MP4 request - SE is crashing after save attempt

PR 9402256: “SE Graphics Test 1" performance test is not running thru completion

PR 9405618: frames get messed up after updating

 

===Draft===

PR 9327095: Dimensions on a sketch disappear when you select a design object, and RMB show only

PR 8393282: added hole gets new hole number although size already exists

PR 8952766: User wants to skip 'define hole table origin' step during placement of new hole table

PR 9382515: Drawing View Wizard Option Crashes session

 

===Part/Sheet Metal===

PR 9173544: Problem with optimized geometry after optimize

PR 9291277: Save as flat DXF options unchecked " Complex Hole" gives wrong result

PR 9357495: Part file crashes while saving in sketch environment

PR 8389690: Region created from sketch with gap

PR 9352716: Move command, as part was moving to a distance double of the dragged distance

PR 9389334: Old generated closed corners cause failure in SE2019

PR 9325163: Abort when trying to move faces in Sync.env

PR 9397714: Construction body fails after linking the material in a design body part copy

PR 9403379: Solid Edge closes after editing pattern in assembly

 

===Translators===

PR 8551634: NX open the JT exported from SE, and the location of PMI dimension is wrong

PR 9304109: Unable to open SolidWorks file

PR 9343819: Not possible to open step file correctly parts missing

PR 9354990: Unable to save as DWG

 

===Data Management===

PR 9351345: Document controllers ignored, only first one can set data obsolete

 

===Teamcenter Integration for Solid Edge===

PR 9227116: LOV value will disappear when saving a new file

PR 9339858: Dynamic LOVs not working

PR 9343658: Teamcenter 12.1 Standard part ignores naming rule

PR 9342992: Assembly JT creation was very slow when wire harness is present

PR 9371297: Error on first Save to Teamcenter of drawing or assembly from active SE 2019 Part

PR 9375450: User must run the Replace Part command twice to successfully replace the part

PR 9383281: Solid edge is crashing randomly

PR 9387708: AddToTeamcenter does not start import of the file if manifest file exists in the directory

PR 9240326: BOM line error with adjustable assembly

PR 9394831: Project removed when revise via Structure-Editor

 

===TechPub===

PR 9304665: Line Break in Illustration description not correct in HTML

PR 9330815: The "Isolate and Zoom" button cannot be activated in the PDF file

PR 9331438: 3D models are sometimes displayed incorrectly in the PDF file

PR 9355213: 3DPub and Illustrations: garbage square after FOA file name in model panel

Regards,
Fred White
Siemens PLM Software
22 REPLIES 22

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi @JFred ,

 

Thanks for your post. I have also a question, I have also Solid Edge Technical Publications, I have to download only Solid Edge MSI MP6, or also download Solid Edge TechPublications MP6?

 

Regards,

 

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Siemens Legend Siemens Legend
Siemens Legend

Sorry about that! The Readme is the correct list of PRs addressed. I have updated the list in the Community posting.

 

Regards,
Fred White
Siemens PLM Software

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Siemens Legend Siemens Legend
Siemens Legend

@Joanpolo There were fixes made in Core Sold Edge as well as in TechPub. So, you will need to download and apply both MPs, the one for Solid Edge and the one for TechPub.

 

Regards,
Fred White
Siemens PLM Software

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thank you. Do you have the readme for the TechPub MP?

Regards,

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Siemens Legend Siemens Legend
Siemens Legend

The PRs addressed are in the main readme file:

 

===TechPub===
PR 9304665: Line Break in Illustration description not correct in HTML
PR 9330815: The "Isolate and Zoom" button cannot be activated in the PDF file
PR 9331438: 3D models are sometimes displayed incorrectly in the PDF file
PR 9355213: 3DPub and Illustrations: garbage square after FOA file name in model panel

 

Regards,
Fred White
Siemens PLM Software

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Legend
Legend

Well, I downloaded the MP6 and tried to install and got the following error.

 

"Error 2705.Invalid table: Directory; Could not be linked as tree."

 

I have tried running as admin, I have tried redownloading and running again and as admin, same thing.

 

SE 2019 MP5

Windows 10 1607 14393.0

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@nanan00  when this error typically occurs it implies that you do not have the correct base build version of Solid Edge installed.

 

Please download the base Solid Edge software again, fully uninstall Solid Edge, then reinstall Solid Edge using the new download, and then apply the maintenance pack.

 

 

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi @uk_dave ,

 

Which is the last base build of Solid Edge?

 

Regards,

Re: Solid Edge 2019 - Maintenance Pack 6 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@Joanpolo the latest one available for download from the GTAC file server. 


There was an incorrect build of the base Solid Edge software upon initial release that was briefly and for a very limited time posted for download on the GTAC server.  That build was then quickly removed and an updated correct build provided.  However the build numbers were not changed.

 

So therefore reviewing build numbers to determine the base software version that presents this issue is not possible.


With that said the base SE2019 version is 219.00.00.091.