Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge 2019 and 3D Space Controller

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,

 

 

just have got an info that 3D Space Controller does not support SE 2019.

 

This answer was given after frequently and regulary crashes of SE2019 (when closing a window) was reported and dedicated to the controller (disableling the controller addin has stopped the crashes immedeately)

 

The arguement by them is, that there were changes in the SE interface of 2019, which they can not handle and what they also do not expect to be able to do in future.

 

Is this something what could be confirmed?

Does anbody else use those devices?

 

Please do not mix up those devices with the 3D connexion space mouse!

 

 

regards
Wolfgang
4 REPLIES 4

Re: Solid Edge 2019 and 3D Space Controller

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad  if the "3D Space Controller" is not a 3Dconnexion device, who produces the device you are referencing?



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge 2019 and 3D Space Controller

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

3D Space Control

 

See following link:

 

We had them in use for years here!

 

https://spacecontrol.de/

 

 

 

Maybe they were more common in the German speaking area.

 

 

regards
Wolfgang

Re: Solid Edge 2019 and 3D Space Controller

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad I have not seen those before.  We use the 3Dconnexion devices and they appear to work fine in SE 2019.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge 2019 and 3D Space Controller

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

Yes this is also what I know, that the 3D connexions do what they should do!

 

 

regards
Wolfgang