Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Solid Edge 2019 is officially released to customers

Community Manager Community Manager
Community Manager

We are working to announce Teamcenter 12 support with the release of Solid Edge 2019 MP1.  Stay tuned for more details later this week.

 

Laura

Solid Edge Release Manager

Re: Solid Edge 2019 is officially released to customers

Phenom
Phenom
@Joris Ha, you funny guy! SW attempted this and it was a big flop!

Re: Solid Edge 2019 is officially released to customers

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Good info Smiley Happy Many Thanks!

Re: Solid Edge 2019 is officially released to customers

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I just got an email that SE2019 MP1 has been released but looks like there is something wrong in the package. I am not able to install it. Can you check if it works for you?

 

SE2019_MP1.png

Re: Solid Edge 2019 is officially released to customers

Community Manager Community Manager
Community Manager

@TauseefAkhtar

If you installed Solid Edge 2019 from 2019/Media DVD/Solid_Edge_DVD_<language>_2019.exe, then MP1 installs fine

 

If you installed via 2019/Solid_Edge_2019.exe, the MP1 install will fail

 

You will need to remove Solid Edge 2019 and install 2019/Media DVD/Solid_Edge_DVD_<language>_2019.exe and the MP1 will install fine.

 

We are actively working to replace the 2019/Solid_Edge_2019.exe now.

 

We deeply regret the inconvenience.

Laura

 

Re: Solid Edge 2019 is officially released to customers

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks alot Laura. 

 

That worked so well with the new package Smiley Happy 

 

Appreciated greatly!

Re: Solid Edge 2019 is officially released to customers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm confused (newsflash), I just downloaded this file: Solid_Edge_DVD_ENGLISH_2019.exe. When I double click it it doesn't extract into separate folders but it runs the install interface.

 

extract2019.JPG

 

Have I finally lost my mind?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge 2019 is officially released to customers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand,

 

Yes my friend, I think you have.... Robot LOL

 

You'd need to use a file compression tool, such as WinRAR [or similar], then simply right click the *.EXE file and choose "Extract Here".

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge 2019 is officially released to customers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@SeanCresswell Well it's official then. I thought when it was described as self extracting when double-clicking that it would do that. 7-Zip appears to be doing it per your instructions. I've done this before so...wow.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge 2019 is officially released to customers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

 

I believe that it is as You thought.

An exceptional zip file might be extracted before - somewhere in the deep of personal folders (%appdata%) , will be executed and obviously deleted automatically after usage.

 

So exactly that is the reason why I extract them manually once and use those folder structures later as often as needed.

This saves the extraction time for every use.

 

But maybe I'm wrong with that.

 

 

regards
Wolfgang