Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Solid Edge 2019 is officially released to customers

Gears Phenom Gears Phenom
Gears Phenom

@hawcad wrote:

Hi @bshand

 

 

So exactly that is the reason why I extract them manually once and use those folder structures later as often as needed.

This saves the extraction time for every use.

 

But maybe I'm wrong with that.

 

 


I exactly do the same, we do have 8 PC to setup and would be time consuming to extract every time.

Re: Solid Edge 2019 is officially released to customers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@LauraWatson wrote:

 

If you installed Solid Edge 2019 from 2019/Media DVD/Solid_Edge_DVD_<language>_2019.exe, then MP1 installs fine

 

If you installed via 2019/Solid_Edge_2019.exe, the MP1 install will fail

 

You will need to remove Solid Edge 2019 and install 2019/Media DVD/Solid_Edge_DVD_<language>_2019.exe and the MP1 will install fine.

 


Well, I'm still confused.

1) I don't see a file named "Solid_Edge_2019.exe" on the download page. Has it been removed?

2) What is the best way to install?

   a) Running the self extracting "Solid_Edge_DVD_<language>_2019.exe"

   b) Extracting "Solid_Edge_DVD_<language>_2019.exe" to show all the dvd folders and then running from

        DVD\Solid Edge\setup.exe or Siemens Solid Edge 2019.msi.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge 2019 is officially released to customers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bshand  "Solid_Edge_2019.exe" was removed because it created a corrupt intall of SE 2019 that could not be patched.

 

The solution was to uninstall and use "Solid_Edge_DVD_<language>_2019.exe".

 

It doesn't matter whether you run the download or use a ZIP tool to extract it to a folder, they both will do the samething when performing an install.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge 2019 is officially released to customers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@KennyG, thanks, makes sense. I figured but it just wasn't clear to me.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge 2019 is officially released to customers

Experimenter
Experimenter

We work in a school and have deployed ST10 in many computers.

 

In case we need to change the version, which should be the scenario?

 

1) The best one. Is possible that both versions work well together? Any doc about it? Any doc about instaling silently 2019?

 

2) If it's not possible that both of them work well together. Is there any doc about silent uninstalation of the complete ST10 version, and then a silent instalation of the newer version?

 

Thanks in advance. Have a good day