Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge 2019, missing toolbar

Genius
Genius

Where is the toolbar?

Tools, view etc.Missing toolbar.png 

Solid Edge 2019
7 REPLIES 7

Re: Solid Edge 2019, missing toolbar

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Looks like an issue with your installation.  Are you using a custom Theme?  If so set to a delivered Theme and if that doesn't resolve it, maybe a clean re-install?



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Solid Edge 2019, missing toolbar

Genius
Genius

Changed the Theme, did not work.

I will try a clean re-install now.

 

Solid Edge 2019

Re: Solid Edge 2019, missing toolbar

Genius
Genius

I restarted  Solid Edge and now I have the toolbar, strange.

 

Solid Edge 2019

Re: Solid Edge 2019, missing toolbar

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Geir-Petter

 

 

I had the same issue and behaviour, but I have forgotten to delete/rename my custom toolbar setting under %appdata%

 

So SE did a copy of all toolbars from "unigraphics\...." to the new folder Siemens\... 

 

So I stopped SE, renamed that folder and started again, where all toolbars/menu where visible again

 

 

regards
Wolfgang

Re: Solid Edge 2019, missing toolbar

Genius
Genius

Missing toolbar_1.png

Could it be this one?

Solid Edge 2019

Re: Solid Edge 2019, missing toolbar

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Geir-Petter

 

 

 

Yes this exactly is the correct folder!

 

I assumed that everybody knows the Windows variable "%appdata%", which brings You to that folder when be entered in the command line of the explorer.

Sorry for that!

 

And this is/was the place where SE saved the user custom settings for his user interface.

And when this folder of an old version is in place, SE copies it when starting a new version the first time.

But then - and this was the case very often - people were missing new features and function in their multi tab menu, or I suppose, had this strange behaviour, we have seen when starting 2019 the first time.

 

 

regards
Wolfgang

Re: Solid Edge 2019, missing toolbar

Genius
Genius

Hi Wolfgang,

This solved my problem.

 

Thank you!

 

Cheers,

Geir

Solid Edge 2019