Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid Edge 2020 is Released!!

Community Manager Community Manager
Community Manager

All,

 

It is with great pleasure that I announce the release of Solid Edge 2020!!  Solid Edge 2020 is another multilingual release – it includes all 14 languages.  Additional Solid Edge 2020 Portfolio products will continue to release over the coming weeks.

 

Solid Edge 2020 (220.00.00.104) will be available for download later next week once all customer license files are available.  Look for the traditional Software Field Bulletin (SFB) announcing its availability for download later next week. We are also actively working to update all other Solid Edge 2020 downloads (i.e. Academic, Trial, Free 2D, Solid Edge Viewer, and so forth), starting later next week.

 

Like Solid Edge ST10 and 2019, Solid Edge 2020 is download-only. DVDs can be requested by emailing dsom.plm@siemens.com, including your customer install number in the email text and “Solid Edge V220” as the email subject.

 

Enjoy!

 

Laura Watson

Solid Edge Release Manager

13 REPLIES 13

Re: Solid Edge 2020 is Released!!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Solid Edge 2020 Help is up.  Here is a link to the What's New section:

https://docs.plm.automation.siemens.com/tdoc/se/2020/se_help#uid:index_newse



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge 2020 is Released!!

Valued Contributor
Valued Contributor

I can't find setup file on site. Why?

Cattura.PNG

Re: Solid Edge 2020 is Released!!

Gears Phenom Gears Phenom
Gears Phenom

Hi @And_M_One ,

 

@LauraWatson wrote this: "Solid Edge 2020 (220.00.00.104) will be available for download later next week" Today is Tuesday! Try it later! Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Solid Edge 2020 is Released!!

Valued Contributor
Valued Contributor

OH SORRY!!!!! Smiley Very Happy

Re: Solid Edge 2020 is Released!!

Community Manager Community Manager
Community Manager

No worries.   IT will be working to revise the many product ids in SAP today from Solid Edge 2019 to Solid Edge 2020.  Once this happens, SAP will email customers their new Solid Edge 2020 license files by zone.  Then we will post Solid Edge 220.00.00.104 for download on the GTAC site.

 

Simultaneously, we are working to get the various free product download sites updated to Solid Edge 2020.  This include Solid Edge Free 2D, Free Viewer, Academic, and so forth.  These products are all built with 220.00.00.104 and tested.  We're just working with other teams to get them updated.

 

We are as anxious as you to get Solid Edge 2020 to our customers, and we are focused on this. :-)

 

Have a great day,

Laura

Re: Solid Edge 2020 is Released!!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@LauraWatson You would think with several months notice and a tentative release time frame, the sales/marketing/accounting teams would have all their stuff ready to go and be able to switch over with the push of a button on the weekend...



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge 2020 is Released!!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@KennyG, you sound like some managers I've worked with. "It's CAD, can't you just push some buttons"? Smiley Happy

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge 2020 is Released!!

Phenom
Phenom

@KennyG To be fair they could have done this all under the radar and in a couple of weeks time just 'pushed the button', and only then tell us what's going on, so at least they're being open and giving us information on the rollout.

Re: Solid Edge 2020 is Released!!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Alex_H @bshand  All I'm saying is that something like licensing could have been all set up last month as everybody knew SE 2020 was releasing this month or beginning of next... Why wait until SE 2020 is actually released to start generating licenses?  It just makes it look like somebody got surprised by a new software release...



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com