Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge BOM structuring

Pioneer
Pioneer

Hey all,

 

"Quick question" on BOM structures in Solid Edge. Coming from Inventor, there was the ability to mark assemblies as "Phantom" - meaning that if you placed the phantom assembly into another assembly, the BOM print out of the parent assembly would appear flat, but the sub-assembly could still be opened and edited independently.

 

For example if you had an assembly with 3 sub-assemblies, one marked phantom (composed of say 4 sub-components), and some number of sub-components, the BOM would come out looking roughly like:

 

Furthermore, would the parts list on a JT file reflect this?

 

Parent Assm

 - Sub-Assm 1

 - Sub-Assm 2

 - Component 1

 - Component 2

 - Component 3 (Phantom Sub-Assm)

 - Component 4 (Phantom Sub-Assm)

 - Component 5 (Phantom Sub-Assm)

 - Component 6 (Phantom Sub-Assm)

 - Component 7

 - Component 8

 

The relevant help page from AutoDesk: https://knowledge.autodesk.com/support/inventor-products/learn-explore/caas/CloudHelp/cloudhelp/2014...

25 REPLIES 25

Re: Solid Edge BOM structuring

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not totally sure I understand your dilemma but look at the "list control" tab in parts list properties and see if that clarifies anything. Also occurence properties on the components in the assembly(s).

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge BOM structuring

Pioneer
Pioneer

The textbook case of "phantoms" in manufacturing are things that have multiple drawing levels, but are not processed or inventoried as an assembly.

 

The simple example is a progressive automotive die where a part will be stamped 3-4 times through different die sets. Each station needs it's own drawing, but there are no inventory moves or transactions beteween the levels because the process is so fast.

 

Similarly bolt/hardware kits are set up as phantoms, where the bolts are stationed line-side, and picked as needed, but in the CAD model the hardware is kitted by assembly function so it can be readily re-used. Marking the bolt kit as phantom allows designers to re-use the same kitted assembly where necessary without pulling in each individual hardware piece. However on a print or BOM the hardware would show up without being under the kit as the total of necessary hardware at that level.

Re: Solid Edge BOM structuring

Phenom
Phenom

@Sathersc86 If you mark an assembly as a weldment (Tools>Weldment) then by default it won't be expanded if you do an assembly report to produce a BOM. Unfortunately it won't prevent the full structure appearing in the JT.

Re: Solid Edge BOM structuring

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Sathersc86, I'm still not clear. Is the "kit" an item in itself in the cad database or just an abstraction?

For instance, part of the definition of phantom in the link is:

 

  • They are ignored by the BOM.
  • They are included in assembly mass calculations
  • They are not numbered, and are not directly included in quantity calculations.

That could be handled in the items occurence properties.

This part I don't follow although:

 

  • They influence the participation of their children in the BOM by promoting them in Structured BOM views. The children of a Phantom component are treated as siblings to the phantom component siblings, even though from a model structure standpoint, they are not.
  • The quantity of their children is multiplied by the quantity of the phantom component.

 

 

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge BOM structuring

Gears Phenom Gears Phenom
Gears Phenom

It's like bringing in a sub assembly that is composed of a bolt, a washer and a nut, but the sub assembly isn't listed in the BOM, but it does expand and list the bolt washer and nut.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Solid Edge BOM structuring

Gears Phenom Gears Phenom
Gears Phenom

Go into "list control" after right clicking your parts list and selecting properties. I believe you want to select your subassembly, tell it to expand it listing it's components.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Solid Edge BOM structuring

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So, if I follow, in list control, at top level select "atomic list", "include" everything below it, and for each subassy "include assembly components".

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Solid Edge BOM structuring

Gears Phenom Gears Phenom
Gears Phenom

No, I'm thinking more like this. In this case, I had the BOM expand the subassembly so it lists all of its components individually, but the subassembly isn't listed.

Capture.PNG

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
Highlighted

Re: Solid Edge BOM structuring

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Interestingly, the result is the same.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200