Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid_Edge_Drafting_Ordinate_Dimension

Builder
Builder

Hello_Guys,

                      I am new in solid edge , In attached Image is that possible to give ordinate Dimension like autocad Break dimension,

 

 

 

 

 

Capture_Broken_Dimension.JPG

                    

If any body have any idea for this ,please share it

Warm Regards
Thomas Roman
Machine Designer
3 REPLIES 3

Re: Solid_Edge_Drafting_Ordinate_Dimension

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

There is no direct equivalent command that I know but here are couple of methods that can take you very close.

1. Use the Coordinate Dimension command, pick the circle center and then change the value to 500:

 

2015June23-02.png

 

2. Use the regular linear (Smart) dimension command and set the Terminator Type to Blank + Check Off Show Dimension Line:

 

2015June23-01.png

 

The second method more closely resembles the image you have shared.

 

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group

 

Re: Solid_Edge_Drafting_Ordinate_Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Thomas_Roman,

 

Further to @Tushar's great options....you can do this, using the coordinate dimensioning command, but, hold the ALT key to place the "alternate" location annotation point, like my image below. [set up a style, to have the leader & arrows, as desired]

 

ST8_DFT_AltOrdinateDims [1].jpg

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid_Edge_Drafting_Ordinate_Dimension

Builder
Builder

Thanks guys thanks for support

Warm Regards
Thomas Roman
Machine Designer