Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Explorer View icons.

 Dear All Masters

 

Dear @Tushar sir

 

 

Thanks To here for Support 

 

I have one Question about Solid Edge Icons On Windows Explorer.

 

Can Solid edge Put Icons Of Moudles Like Part ,assembly,Sheetmetal ,weldment , on Thumbnail So if We have settings on large icon So we can Understand Which File Is this ..

 

 

solid edge only showing Solid edge Application icon on thumbnail

 

I have attached images of it..

IMG_20160611_214110_1465697505415.jpgIMG_20160611_185726.jpg

 

1 REPLY 1

Re: Solid Edge Explorer View icons.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Dear Vrushank:

  

Further to what mentioned in the other post, I believe you will have to figure out the file type based on either the thumbnail preview or only the icon. Both preview and file type icon does not seem possible at same time.

     

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group