Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Help on the Web

Experimenter
Experimenter

I'm new to Solid Edge and have just downloaded ST9.

 

The help file says, "The web-based training is only available when you turn on the Solid Edge option (on the Helpers tab of the Options dialog box) to Use my web browser to display help."

 

However, that option is not available in the Helpers tab.  Did that go away with ST9?  Or is it available elsewhere?

3 REPLIES

Re: Solid Edge Help on the Web

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No, still where it says it is.  Don't forget to scroll to the bottom of the form.

 

Web based Help is the default by the way.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Solid Edge Help on the Web

Experimenter
Experimenter

I did scroll to the bottom of the form.  The last item on the form is:

 

"Document Name Formula"

 

There is nothing below that.  Did I get an erroneous download perhaps?

Re: Solid Edge Help on the Web

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Don't know.  It's there on mine but I do have the full commercial license.  If you are using the Free 2D license, they may shut off that option.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com