Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge License Manager in Windows server 2016 std OS

Experimenter
Experimenter

Hi,

   When can we expect the develoment to use solid edge license manager to work with Windows Server 2016 std Operating system.

 

Thanks & regards

Mahesh

7 REPLIES 7

Betreff: Solid Edge License Manager in Windows server 2016 std OS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @maheswaran

 

 

 

is this a problem?

 

IT is going to upgrade and if license server will not run .....

regards
Wolfgang

Betreff: Solid Edge License Manager in Windows server 2016 std OS

Siemens Phenom Siemens Phenom
Siemens Phenom

Windows Server 2016 is not a supported platform with the underlying FlexNext Publisher 11.14 software.  

Betreff: Solid Edge License Manager in Windows server 2016 std OS

Legend
Legend

@uk_dave

 

Windows Server 2016 not supported...
Strange... I run a Windows Server 2016 with the FLEX LM tools serving my SE licenses (including TC).

Could be that this works as it is MAC/CID instead of the good old dongle ;-)

 

 

--------------------------------------------------
Marc Boom
marc.boom@outlook.com

Betreff: Solid Edge License Manager in Windows server 2016 std OS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @marcboom

 

 

till now it was working since the server did not know that it must not work,
but just now we have sold the pass that it is not allowed to do so.

 

Smiley Tongue

regards
Wolfgang

Betreff: Solid Edge License Manager in Windows server 2016 std OS

Siemens Phenom Siemens Phenom
Siemens Phenom

@marcboom "not supported" is *not* the same as "running".

Betreff: Solid Edge License Manager in Windows server 2016 std OS

Siemens Phenom Siemens Phenom
Siemens Phenom

@hawcad nor is "not supported" the same thing as "not allowed".

Highlighted

Betreff: Solid Edge License Manager in Windows server 2016 std OS

Legend
Legend

@uk_dave

 

100% correct...
Some you just need to give it a try.... Smiley Very Happy

--------------------------------------------------
Marc Boom
marc.boom@outlook.com