Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge License Type Feature Comparison ... Where find the table ?

Valued Contributor
Valued Contributor

Hi guys

 

Where I can get the table with the features x license types  for ST10 ?  (Including the new aplications and features that comes w it)

 

Thanks

---------------------------------
Hilario, Flavio
Industrial Designer
ST10 / Win10
5 REPLIES

Re: Solid Edge License Type Feature Comparison ... Where find the table ?

Phenom
Phenom

Here you go. Page 2 has a chart.

Re: Solid Edge License Type Feature Comparison ... Where find the table ?

Valued Contributor
Valued Contributor

Hi @RyanM

Thank for your quick reply.

 

I found a more recent table here on our Knowledge Base sub-forum  : https://community.plm.automation.siemens.com/t5/Solid-Edge-Knowledge-Base/Solid-Edge-License-Type-Fe... (The one you posted is from 2014, or both could be even from the same source)

 

I am still trying to find one about ST10 . I see a lot of "What's New' documents and pages over internet .. but none contains that table.

 

BR

---------------------------------
Hilario, Flavio
Industrial Designer
ST10 / Win10

Re: Solid Edge License Type Feature Comparison ... Where find the table ?

Valued Contributor
Valued Contributor

That seems to be the most recent one (2017)

 

https://www.plm.automation.siemens.com/media/store/en_us/Siemens-PLM-se-Features_tcm29-1997.pdf

---------------------------------
Hilario, Flavio
Industrial Designer
ST10 / Win10

Re: Solid Edge License Type Feature Comparison ... Where find the table ?

Honored Contributor
Honored Contributor

I would like to ask a very related question rather than starting a new thread.

 

What is included with the "part's library"

Since I use foundation, I don't know.

Re: Solid Edge License Type Feature Comparison ... Where find the table ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@12GAGE  The Classic and up licenses includes the Machinery and Piping libraries.

 

Solid Edge Machinery and Piping Libraries

In addition to the baseline of components delivered with Solid Edge, additional libraries are available as optional add-on packages:

The Solid Edge Machinery Library contains thousands of components that support a growing range of international standards (ANSI, DIN, ISO, AFBMA, AISC, UNI, JIS, GB).

The Solid Edge Piping Library contains an extensive selection of standard fittings, including elbows, bends, returns, Ys, tees, and reducers, as well as a large collection of essential components such as flanges, unions and seals. Fittings are available in a variety of relevant end treatments, such as threaded, welded, flanged and slip-on.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com