Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge On-Line Help Problem

Phenom
Phenom

I am getting the following error on two computers when I try to go to on-line SE help. Anyone else see this? Know of a fix?

 

Thanks,

 

Error.jpg

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317
4 REPLIES 4

Re: Solid Edge On-Line Help Problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Bob,

 

Yup, seeing this too......must be a server issue.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge On-Line Help Problem

Phenom
Phenom

Ok, so a server issue with them and not something wrong on my workstation.

 

What I was headed to help for was a quick tutorial on rendering with Keyshot. I have not used it yet and I was asked today to create about 25 images for marketing. Nothing fancy, and I could have done it quickly and easily in the old rendering environment, but now I am completely lost.

 

Does anyone know of anything on line in regard ot keyshot tutorials. Just need to get some quick images and I don't have a lot of time to spend learning at the moment.

 

TIA

 

 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Solid Edge On-Line Help Problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Seems to be working now Bob.

 

Only have my learners permit with Keyshot myself. Robot Embarassed

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge On-Line Help Problem

Honored Contributor
Honored Contributor

If the on line help works or not appears to me to be dependent on the total strength of Internet connection + the load on the Siemens server. If the request times out, that is the error.

 

A work around is to capture the links when it does work, then place that link in chrome that tends to have less lag. That helps me over half the time, but not all the time depending on your access and the total Internet load.