Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Option define permanet Arc smoothness

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

 

Is it possible to define permanent number on arc smothness in Solid Edge Options. When I change this from 3 to 10 it will always return to default number ( 3) after closing SE.

 

 

 

 

1 REPLY 1

Unfortunately, Arc Smoothness in the options only 'sticks...

Phenom
Phenom

Unfortunately, Arc Smoothness in the options only 'sticks' for the current Solid Edge session. Additionally, the Sharpness setting (Blue segmented circle) under the View tab, which also affects visual display, is reset to '2' (of 5) every time a document is opened. I think there's an enhancement request for this behavior to be changed that dates back to ST4 or ST5.

-Dylan Gondyke