Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Performance Testv1.2

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,




i want to bring this issue back again.

 

I have run the new SE_Performance Test v1.2 with ST10 on my computer, where I also have all the result from the last years, with results of performance test v1.0 from ST6/7/8/9

 

So of course I'm awamre about thefaact that I should use the v1.2 version for ST10 onwards.

 

But what I have seen is one big issue concerning the graphics results which are approx. 3 times as much as previous values.

 

So my assumptions now are either their is a change in testing, to result in these numbers or there is a big slowdown with my graphics, even I have not changed anything on my computer besides ST9 to ST10.

 

The problem now - and this is my post issue - there are no comparison values for this v1.2 test available.

So man can not know wether the test will use different files and routines or the software slowed down.

 

Edgers, can You provide Your experiences and results so that we will have a current state of comparison charts to kno where our computers need help, updates and tuning.

 

 

Here are my first values of v1.2 with ST10 under Win10:

 

 

--------------------------------------------------------
Date: 12.01.2018 18:14:07
Solid Edge Version: 110.00.03.03 x64
Number of iterations: 1

SE Graphics 1: 305,0 Seconds

SE Processor 1: 80,3 Seconds

SE Processor 2: 30,1 Seconds

SE File I/O 1: 101,5 Seconds

SE File I/O 2: 24,1 Seconds

Solid Edge Start Time: 5,7 Seconds

Total: 611,0 Seconds

 

 

It would be fine, if we can get global comparison values for the v1.2 test

 

I always used the old test to improve hardware of our users, and the test helped a lot to see exactly where the problem areas are.

 

 

regards
Wolfgang
25 REPLIES 25

Betreff: Solid Edge Performance Testv1.2

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,

 

 

 

PS.: the above numbers are only from ONE single loop, so You have to multiply it by 3 for comparing it to the old chart values.

 

 

regards
Wolfgang

Re: Solid Edge Performance Testv1.2

Legend
Legend

Hi, if you are reffering to overall SE performance then your are correct and  since I moved to Solid Edge ST10 MP3 it is really slow for me and I'm not sure why. The OS, is win10 pro. build: 16299.192 version: 1709 I held up the fall edition update based on what I saw in earlier postings

 

I'm still learning SE so I make a lot of mistakes mainly with my work flows from other programs being applied here.

 

I'll be following this thread

 

My Dell PC is a

Intel(R) Core(TM) i7-7700K CPU @ 4.20GHz

32Gb Mem 

NVIDIA Quadro M4000 w/Latest Driver


Bob HaskinThanks

Pacific Design Service

Re: Solid Edge Performance Testv1.2

@rbhaskin

 

I was a little unclear about your statement that you "held up the fall edition update based on what I saw in earlier postings." Version 1709 is the Fall Creators Update and it definitely slows down Solid Edge - particularly dialog boxes with a lot of icons - like the call-out properties dialog box in draft.

 

I got so frustrated with v1709 that I reinstalled Windows 10 and went back to v1703 which is much faster. I have seen other forum posts that Microsoft is working on a fix that may be released by the end of this month. We'll see.

 

 

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10

Re: Solid Edge Performance Testv1.2

Legend
Legend

Here are my first values of v1.2 with ST10 under Win10 Build 1607 anniversary update (NOT FALL CREATOR UPDATE):

--------------------------------------------------------
Date: 15.01.2018 08:32:29
Solid Edge Version: 110.00.03.03 x64
Number of iterations: 1
SE Graphics 1: 85,7 Seconds
SE Processor 1: 59,8 Seconds
SE Processor 2: 23,2 Seconds
SE File I/O 1: 70,3 Seconds
SE File I/O 2: 14,5 Seconds
Solid Edge Start Time: 4,3 Seconds
Total: 308,8 Seconds

System:
CPU, Watercooled Intel Core i7 7700K @ 4.70GHz 34 °C
RAM, 32.0GB Dual-Channel @ 1067MHz (15-15-15-36)
Motherboard, Gigabyte Technology Co. Ltd. Z270X-Gaming 7 (U3E1) 28 °C
Graphics, 4095MB NVIDIA Quadro M4000 (HP) 46 °C
Storage, 476GB Samsung SSD 960 PRO 512GB

Kind regards,


Jan Bos
Emmen, The Netherlands

Re: Solid Edge Performance Testv1.2

Valued Contributor
Valued Contributor
Where do you find this test program?

Thanks,
Guy

CAD/CAE Manager
SE2019 MP5

Re: Solid Edge Performance Testv1.2

Valued Contributor
Valued Contributor
Also, are we expecting to see a performance hit with SE due to the recent CPU vulnerabilities which need to be patched?

CAD/CAE Manager
SE2019 MP5

Re: Solid Edge Performance Testv1.2

Legend
Legend

Re: Solid Edge Performance Testv1.2

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Jan_Bos

 

 

 

thanks for sharing YOur results with us.

 

Let me ask one additional question about this:

 

Do You have old results with v1.0 and ST9, ST8 on the same machine?

 

regards
Wolfgang

Re: Solid Edge Performance Testv1.2

Legend
Legend

Hallo Wolfgang,

 

Leider nicht..  No... no results on V1.00

 

Kind regards,

 

 

Jan Bos