Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Piping Routing Error

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

 

I have a problem. I installed the pipping library, I made the processes as in the procedure, but when I start the piping route it takes a lot to open and the message "unable to find any standard in the database" appears. If I try to indicated the pipping part the message "this part is not a standard part" is displayed. The stand parts works ok, just only in the pipping I have this problem. And the same happens with my friends Solid Edge.

5 REPLIES 5

Betreff: Solid Edge Piping Routing Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Felipe_Oliveira

 

 

 

do you have the Piping Library licensed too?

This is an extra module which must be licensed extra too.

 

 

regards
Wolfgang

Re: Solid Edge Piping Routing Error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi @Felipe_Oliveira,

 

Have you set up correctly the Standard Parts Data Base?

 

Please, check in the program "StdPartsSetup.exe" if it is choosen. This program is on C/Program Data/Solid Edge STx/Program

 

Regards,

Betreff: Solid Edge Piping Routing Error

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi @hawcad 

 

I use the Reseller license for Solid Edge, wich is included the Expresroute, Standard Parts. 

 

Felipe

Re: Solid Edge Piping Routing Error

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi @Joanpolo,

 

Yes, it's ok.

 

My Standard parts works correctly, I just have this issue with the Piping.

 

 

Regards,

 

Felipe

Re: Solid Edge Piping Routing Error

Legend
Legend

Hello @Felipe_Oliveira,

have you try first to create a simple pipe with xpresroute?

 

Best Regards

Wolfgang