Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Solid Edge ST-6 crashing - Not able to work

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

  we have installed solid edge ST6 in windows 8 , but it getting closed when we try to open any of the template [part/sheet/assy/draft]. Attaching screen shot for your reference.

 

Note: Actually it's Win 10 Enterprise Operating system & As ST6 was not supported to Win 10, OS Compatability setting was changed to Windows 8. 

 

my query is, will solid edge St6 works on this setup, any possibilities?  (or) we need to change the OS to Win 7/win 8. 

 

4 REPLIES

Re: Solid Edge ST-6 crashing - Not able to work

Siemens Phenom Siemens Phenom
Siemens Phenom

Downgrade your OS

Re: Solid Edge ST-6 crashing - Not able to work

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

@uk_dave

 can you please let me know what are the supporting OS for solid edge ST6

Re: Solid Edge ST-6 crashing - Not able to work

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Maheshwaran

 

 

AFAIR ST6 should work properely with win 7 and win 8

 

Besides that take a look into the installation DVD folder of ST6.

Normally there is a README.HTM file 

 

Here is a screeshot from my ST6 readme.htm but this is from the German DVD

But You can see that Win7 and Win 8 are supported.

 

20170520_1723.PNG

 



regards
Wolfgang

Re: Solid Edge ST-6 crashing - Not able to work

Phenom
Phenom

Even with the compatibility options set to Win 8, you're still running an old version of SE on Win 10 which is not supported. The compatibility stuff in windows is not always great.

 

If it's an option, I'd recommend you upgrade your SE rather than downgrade your OS, as you get the benifits of the improvements in both pieces of software, and the SE upgrade is "free" assuming you're paying maintainance.