Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Phenom
Phenom

What's about this???

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

This is weak point of the Win 10 (it has lots of...), because it doesn't provide folder structure in start menu... Smiley Sad Those icons and commands are coming from "Choose PDM Integration" app.

 

@uk_davefrom my side everything was ok. Smooth downloading and installing...

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

 

 

 

no, in Win10 there is also a folder structure behind the entries in the start menu

 

 

Go to 

 

C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Solid Edge ST10

 

Here You will find all those entries and You will be able to delete whatever You do not want to see here

 

regards
Wolfgang

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Gears Phenom Gears Phenom
Gears Phenom

@hawcadmy friend, I wrote this: "...because it doesn't provide folder structure in start menu". Yes, I know that it's in the background, but I'm not happy with it. "The program tree" is linear and too long instead of using sub-folder like in Win7...

 

This is my opinion... Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

 

 

sorry for missunderstanding.

 

I thought You would like to delete certain entries here to shorten the start menu

regards
Wolfgang

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

 

 

the onyl You can do here is to move the subfolders from Solid Edge ST10 up to the "Programs" folder and - what I did - rename it to e.g. Solid Edge Data Prepare and so on.

Let all begin with Solid Edge to have them each under the next

 

 

Then all those Solid Edge subfolders with programs will be parallel to the Solid Edge ST10 folder

 

It is not perfect but it shortens the lsit within Solid Edge

 

regards
Wolfgang

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Windows 10 Start Menu will no longer display shortcuts in sub-folders under a root folder entry for a particular application.  I "pin" my apps that I use frequently to the Start pane as a Tile so they are more accessible.

 

2017-09-28_8-46-07.png

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

Yes a good answer.

This is what many already have done for office and other applications, and I did for EDGE also, but not for the various edge sub applicastions

On the other hand, most of them are not used so often.

 

regards
Wolfgang

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@xeniaturon please confirm what version including build number of Solid Edge you current have installed.

 

Go to "Learn Solid Edge" tab -> "About Solid Edge".

 

If your version string is not 110.00.00.107 then you do not have a released copy of ST10 installed.

Re: Solid Edge ST10 - Maintenance Pack 1 Announcement

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi, @uk_dave

 

we have the 110.00.00.105 version. Now we tried to install the other version.

 

Thanks.

Xènia