Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST10 - Maintenance Pack 13 Announcement

Siemens Legend Siemens Legend
Siemens Legend

April 24, 2019

 

Dear Solid Edge Customer:

 

Solid Edge ST10 Maintenance Pack 13 is now available for download.

 

Sincerely,

The Solid Edge Team

 

 

=====================

Maintenance Pack Version:

=====================

 

Solid Edge ST10 MP13

Version: 110.00.13.06

 

================

Download Location:

================

 

Solid Edge ST10 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST10/Maintenance_Packs/

 

==========

Installation:

==========

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
  • MSI Product Updates are all-inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
  • MSI Product Updates calculate free disk space before installing. Please be patient.
  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
  • Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
  • When uninstalling, the original source media must be available to allow the recovery of previous file versions.
  • The current MSI Product Update will be the only Update listed and available for uninstallation.
  • After the current Product Update is uninstalled the previous Product Update will become the current Update.
  • .zip files delivered with this MP such as SESP_Server_2010_MP4.zip, SESP_Server_2013_MP4.zip, and SEECAdministratorV110.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

 

For details on initiating your email subscription navigate to:

https://www.plm.automation.siemens.com/global/en/support/email-subscription.html

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===Assembly===

PR 9316364: Cannot change length and suppression variable together

PR 9329260: Crash when reordering multiple group items into another group

PR 9370521: Assembly relationships are broken in top level when editing sub with assembly features

 

===Draft===

PR 9318362: Dimension radius not displaying correctly

PR 9382515: Drawing View Wizard Option Crashes session

PR 9265668: The specified template cannot be accessed. Please specify another template.

 

===Part/Sheet Metal===

PR 9173544: Problem with optimized geometry, that causes problems after optimize

PR 9395289: Crashlog abort resolved in the Select tool

 

===Applications===

PR 9119041: Engineering reference – Gear Tooth thickness of compensation gear should be thicker than general gear

PR 9261665: Engineering reference – Updating a Spur gear, the pinion and gear components are getting interchanged

 

===Translators===

PR 8329150: DWG dimension lines are not trimmed when imported

PR 9290085: Multibody does not show up in Parasolid conversion

PR 9354990: Unable to save as DWG

 

===Teamcenter Integration for Solid Edge===

PR 9308247: SESE aborts when clicked on revise selected

PR 9315592: Project assign is cleared when uploading without displaying the CPD.

PR 9315778: Switching "Show View" to "Parts List" in SESE aborts 

PR 9339858: Use SE MP12 still not support dynamic list of values

PR 9383281: Solid edge is getting crash randomly

PR 9387708: ATTI does not start the import of the file if manifest file exists in the directory

PR 9406962: SaveAs fails if target ASM contains PAR which different rev is C/O to the cache.

PR 9394831: Project removed when revising via structure editor

PR 9384656: Clear attributes on SaveAs (Do not map NULL) does not work for Inter Parts Link data

PR 9402248: User Settings does not work like RAC and requires the command to run 2x to complete

PR 9323959: Preference SEEC_Enable_MultipleRevision=1 breaking Solid Edge links.

PR 9309476: Tc Project Update On Other User Data Is Displaying Error Message In SE

PR 9342992: Assembly JT creation is very slow when a harness is present

PR 9240326: BOM line error with adjustable assembly

PR 9428205: Solid Edge crashed while doing Multi - body Publish

Regards,
Fred White
Siemens PLM Software
3 REPLIES 3

Re: Solid Edge ST10 - Maintenance Pack 13 Announcement

Phenom
Phenom

Hi @JFred ,

 

I can't find any more about PR 9323959 (Preference SEEC_Enable_MultipleRevision=1 breaking Solid Edge links) on GTAC, from the headline it sounds like it might fix an issue we've been having.

 

Could you direct me to where I can see more information please?

 

Thanks.

Re: Solid Edge ST10 - Maintenance Pack 13 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@Alex_H  from the PR notes...


Description:
------------
Description: The preference SEEC_Enable_MultipleRevision with value 1 enables opening multiple revisions of the same part number in Solid Edge. But in some cases, our customer has identified that the links of a Solid Edge assembly or draft can break due to the renaming of the files downloaded to the SEEC cache. We have been able to reproduce the issue in our own setup and we have recorded a short video to show you a possible (likely not the only one) workflow that leads to the breaking of links between Solid Edge assemblies and parts.

 

Steps To Reproduce:
-------------------
1. Set SEEC_Enable_MultipleRevisions to 1
2. Create an assembly and add the first revision of a part to it
3. Open the assembly as Precise (or Latest Working) in Solid Edge
4. Open the second revision of the part in Solid Edge
5. With the second revision still opened, replace the part in the assembly for its second revision
6. Save, check in and close the Solid Edge opened files.
7. Clear the cache
8. Reopen the assembly as Precise, it will report missing files.

 

Additional Note:
----------------

As I mentioned earlier, we do not think this is the only way to reproduce the issue, but it is the easiest way I have found to do so. The 7th step is critical, because if the cache is not cleared, the renamed file still lays there and the assembly will open normally. Our customer first noticed the issue when another user (different from the original designer) tried to open an affected assembly, the original designer could open it normally, but any other user got the missing files dialog shown on screen.



Re: Solid Edge ST10 - Maintenance Pack 13 Announcement

Phenom
Phenom

Thanks @uk_dave , that's exactly what we were seeing but I couldn't work out how to replicate like this user has.