Dear Solid Edge Customer:
Solid Edge ST10 Maintenance Pack 2 is now available for download.
Sincerely,
The Solid Edge Team
============
Release Notes:
============
Solid Edge ST10 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
=====================
Maintenance Pack Version:
=====================
Solid Edge ST10 MP2
Version: 110.00.02.03
================
Download Location:
================
Solid Edge ST10 Maintenance Packs can be downloaded from:
==========
Installation:
==========
Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be
uninstalled using Uninstall a program from the Control Panel.
• MSI Product Updates can be applied on top of the base release and or existing Product Update
with a lesser version.
• MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered
in MP1 and MP2.
• MSI Product Updates calculate free disk space before installing. Please note that there have
been cases where the Disk Space Computation takes several minutes to complete. Please be patient.
• MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
• Uninstalling an MSI Product Update will restore the installation to the state before the Product
Update was applied.
• PLEASE NOTE: When uninstalling an MSI Product Update, the original source media and the previous
Product Update package, if any, must be available to allow the recovery of previous file versions.
• The current MSI Product Update will be the only Update listed and available for uninstallation.
After the current Update is uninstalled, the previous Update will become the current Update, if
there were multiple Updates installed.
• MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed
updates -> Uninstall).
===============
E-mail Notification:
===============
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail
notification.
For details on initiating your email subscription navigate to:
=========================================
This Maintenance Pack addresses the following PRs:
=========================================
===Part/Profile/Sheet Metal===
PR 8970142: SE Crash when exiting FOP
PR 8975139: Result of Generative Design is different between English and Japanese
PR 8993487: Helical Curve with a number of turns < 1 is incorrect.
PR 8975910: Edge crashes when changing material properties.
PR 8994736: Material Table Import does not read Excel files
===Assembly===
PR 8856499: Occurrence property overrides are incorrect when obtained from automation
PR 8920113: SE-User defined mass not carried into upper-level assembly
PR 8986854: FrameComponentUtility.exe brings up a blank dialog.
===Draft===
PR 8965535: User-defined mass for frames is not correct in a parts list.
PR 8965910: Position of dimension moves, when opening ST4 draft in ST9
PR 8981098: Sectioning is failing in certain cases
PR 8984946: Tolerance Table does not work for smart dimensions along 2 edges
PR 8985069: Broken view becomes un-broken when opened in ST9
PR 8986475: Hole label position changes after an update, regression against ST9.
PR 8962304: Hole Table and Save As Translated issues in ST10.
PR 8985129: The border of callout disappears when opening the data of ST4 in ST9.
===Translators===
PR 8902860: Callout is moved after saving as DWG
===API===
PR 8350832: ActiveDocument under Iapp gives nothing with a 2D Drafting license
PR 8936580: automated explode config application throwing an exception.
PR 8993987: SEPropertyHandler.dll is changing thread locale
===General===
PR 8972970: Problem saving new file w/ file already exists
===Teamcenter Integration for Solid Edge===
PR 8975742: SEEC: Enable TcServer Logging at SEEC Login
PR 7767962: The last_released_status property does not map correctly in SEEC
PR 8350891: In cache assistant, some commands are grayed with a 2D drafting license M
PR 8994811: Copy and paste from AWc to Asm does not work
===Built-in Data Management===
PR 8964054: Problem with Where-Used (BiDM) - does not work permanently
===Design Manager===
PR 8929204: No Duplicates found for part saved in local folder and duplicates on server