Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST10 - Maintenance Pack 4 Announcement

Siemens Legend Siemens Legend
Siemens Legend

February 12, 2018

 

Dear Solid Edge Customer:

  

Solid Edge ST10 Maintenance Pack 4 is now available for download.

 

Sincerely,

The Solid Edge Team

  

============

Release Notes:

============

 

Solid Edge ST10 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

 

Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.

 

=====================

Maintenance Pack Version:

=====================

 

Solid Edge ST10 MP4

Version: 110.00.04.03

 

================

Download Location:

================

 

Solid Edge ST10 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST10/Maintenance_Packs/

 

==========

Installation:

==========

 

Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be uninstalled using Uninstall a program from the Control Panel.

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
  • MSI Product Updates calculate free disk space before installing. Please note that there have been cases where the Disk Space Computation takes several minutes to complete. Please be patient.
  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
  • Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
  • PLEASE NOTE: When uninstalling an MSI Product Update, the original source media, and the previous Product Update package, if any, must be available to allow the recovery of previous file versions.
  • The current MSI Product Update will be the only Update listed and available for uninstallation. After the current Update is uninstalled, the previous Update will become the current Update, if there were multiple Updates installed.
  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

 

For details on initiating your email subscription navigate to:

http://support.industrysoftware.automation.siemens.com/general/email.shtml

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===General===

PR 9018172: Menu / Icon load slow after installation of Windows 10 Fall Creator Update

PR 9058022: No longer able to use stylus after updating to Windows 10 Fall Creator Update

PR 8536218: Saving Solid Edge files fails when there is no disk space, should provide warning

PR 9067490: Switching between windows takes many, many seconds

PR 9079004: Solid Edge properties are missing in Windows Explorer after installing ST10MP

 

===Assembly===

PR 8969056: Profile relationships lose connection and do not update

PR 7601296: Physical properties, update on file save does not work

PR 8358219: Solid Edge aborts when showing sketches in assembly

PR 8993495: Reference plane does not update when linked excel variable changes

PR 9011878: frames created are totally wrong

PR 8996483: Holes are changing if OTHER holes are changed

PR 9059608: 3D Sketch displays for inactive simplified subassembly

PR 9062219: Transparency in Texture background color function does not work correctly

 

===Draft===

PR 8352907: Detection of paper orientation when printing does not work in ST10

PR 7927673: More than 30s to modify line width or color in a group

PR 8351407: Undesired spaces in the stacked text

PR 8356263: Cannot drag columns of block table with ALT key in 2D Model view

PR 9013569: Hole Table annotation moves to default position if one hole will be removed

PR 8957087: Coordinate dim on rotated view is incorrect

PR 9009961: A modification that succeeds in MP9 fails in MP10.

PR 9016318: Broken out section does not cut correctly

PR 9024961: Crash when copying from background sheet

PR 9041036: Unnecessary hatch is displayed when drawing data of ST4 is opened in ST9

PR 9045466: Vertical dimension changes when trying to reattach witness line endpoints

PR 9069626: Wrong units shown in print range on Paper Print settings dialog

 

===Part===

PR 9008477: After creating a block the active layer does not change and hiding layers does not work

PR 9008495: Suppressed or rolled back features affects the features created previously

PR 9011611: PMI Dimension not showing Status correctly

PR 9019993: Members of FOP are opening only in preview

PR 9021121: "IF" formula doesn't work properly in Variable Table

PR 9043412: XpresRoute gives an error when using saved setting end treatment of 90 deg

PR 8935862: Failed to optimize selected geometry

PR 8981720: Recompute fails

PR 9036131: Flat pattern not creating with normal cut on lofted flange

 

===Translators===

PR 8356404: Some graphic components are not imported from AutoCAD

PR 8982501: Catia translator fails to open part

PR 8987714: SW drawings imported into Solid Edge are different

PR 9004389: Abort, when trying to open DXF Files

 

===API===

PR 9021063: Please add new method BindKeyToTopology to Occurence/SubOccurrence object

PR 9007849:  Rotate and other view manipulations become slow after execution of user API

PR 9069254: Request the SolidEdgeDocument.Name API include write/set capability

PR 9007760: Call to API methods in custom AppDomain

PR 9008679: GetLengthAtParam() throws unspecified error in ST9

 

===Illustrations & 3D Publisher ===

PR 9056205: Tech Pub license features do not enable D&D functionality

PR 9031948: Solid Edge Technical Publications cannot output Chinese in PDF

PR 9037247: Technical Publication update doesn't check for existing installation

 

===Built-in Data Management===

PR 9005799: Revision number is not automatically set in new document window using built-in

PR 9027586: Unable to revise if a dot "." is in the path name

PR 9030796: ST10 Property Manager - status greyed out

PR 9061202: Get Latest Released gets the wrong revision

 

===Design Manager===

PR 9058390: FOP child part incorrectly moved from Standard Parts to released

 

===Insight===

PR 8956565: Insight: Insert assembly copy does not allow me to create new mirrored parts

PR 9028381: Insight: SE - Last saved location is not remembered in File save dialog

 

===Teamcenter Integration for Solid Edge===

PR 9030895: XpresRoute failures; no Material and error displayed

PR 8950787: Open dialog Files of Type field changing.

PR 8989772: No SE save_prompt closing asm after changing occurrence property via API

PR 9019859: Custom mapped required attribute is not using the custom property from SE file

PR 8356741: TALLOG message "The New component to be added during BOM Sync is ...

PR 8541999: Failed while saving if SEEC cache folder name has Korean character

PR 8942515: Create Part in Place does not honor the material selection defined by user

PR 8970920: PDF is checked out in TC and save of draft gives non-related error

PR 9013888: SE Status User Display property not changed when status updated via automation

PR 8358182: CPD does not render custom props in case of predefined Item Type

PR 9053765: Add to Teamcenter - Interactive, Item Name / Title mapping problem (Spanish)

PR 9060879: Open draft cmd will not find .dft if there is no GRM

PR 9062383: Mass is changing from lbm to kg when saving into TC

PR 9027216: Revise is changing the author in draft files to whoever revised

PR 9065345: Where used will not find dft with no GRM in the same item rev w\linked par

Regards,
Fred White
Siemens PLM Software
29 REPLIES

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Legend
Legend

Thanks for the maintence pack and the recompute fix!

 

But there is a bug in the maintence pack all filled options are empty in balloons and dimensions. Can this be fixed asap with a new build before I deploy this within my company? All old placed  balloons and dimensions are infected to by the way.

 

Filled broken ST10 MP4.PNG

Sander
The Netherlands

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Legend
Legend

I'm also affected by this bug..2019.jpgFilled arrow and balloon dot bug

Assume that this will be corrected in MP5  and that the filled arrows and dot at the end of an balloon are back... and not gone forever.

 

Please confirm,

 

Kind Regards

 

Jan Bos

Emmen, The Netherlands

 

 

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Legend
Legend

There are not gone, if I order our server to make PDF they are still filled but that one runs MP3.

 

Filled broken ST10 MP4 PDF.PNG

 

This MP fixes some important bugs which costs time, to break something else I do hope they will not let us wait 6 weeks minimum.

 

Cheers,

Sander

Sander
The Netherlands

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Gears Phenom Gears Phenom
Gears Phenom

Please...

How is this possible?????

 

Isn't a MP tested? Just open a draft and you see this. Unbelievable!

Smiley Mad

 

above: pdf

under: dft

jMIRQEd

 

http://allyplm-solutions.blogspot.be/2016/03/solid-edge-tip-of-week-how-to-uninstall.html 

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Legend
Legend

Filling is just broken as it is.

 

Here is selected filling of the P and it's filled black but shown empty. Why is the G and I filled?

Filled broken ST10 MP4 filling.PNG

Sander
The Netherlands

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Legend
Legend

Bug has been reported.

 

Siemens ID 9086877.

De status van deze call is nu Siemens (IR). Dit betekent dat Siemens deze Incident Report in behandeling heeft als zijnde High priority.

Sander
The Netherlands

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Phenom
Phenom

@Sander-NL

Because the G and i don't have internal areas, just one outline ?

Same as the b and o on @Joris 's image.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Phenom
Phenom

the same issue on my SE.

 

Arek

Re: Solid Edge ST10 - Maintenance Pack 4 Announcement

Legend
Legend

And I wanted to start shouting already to some people.... Smiley Very Happy

 

 

--------------------------------------------------
Marc Boom
marc.boom@outlook.com