Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST10 - Maintenance Pack 8 Announcement

Siemens Legend Siemens Legend
Siemens Legend

June 11, 2018

 

Dear Solid Edge Customer:

 

Solid Edge ST10 Maintenance Pack 8 is now available for download.

 

Sincerely,

The Solid Edge Team

  

============

Release Notes:

============

 

Solid Edge ST10 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

 

Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.

 

=====================

Maintenance Pack Version:

=====================

 

Solid Edge ST10 MP8

Version: 110.00.08.04

 

================

Download Location:

================

 

Solid Edge ST10 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST10/Maintenance_Packs/

 

==========

Installation:

==========

 

  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
  • MSI Product Updates calculate free disk space before installing. Please be patient.
  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
  • Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
  • When uninstalling, the original source media must be available to allow the recovery of previous file versions.
  • The current MSI Product Update will be the only Update listed and available for uninstallation.
  • After the current Product Update is uninstalled the previous Product Update will become the current Update.
  • .zip files delivered with this MP such as SESP_Server_2010_MP4.zip, SESP_Server_2013_MP4.zip, and SEECAdministratorV110.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.

 

For details on initiating your email subscription navigate to:

http://support.industrysoftware.automation.siemens.com/general/email.shtml

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===General===

PR 9115312: Server busy messages on Windows 10 Fall Creators Feature Update

 

===Assembly===

PR 9139880: Can no longer enter Title, Description & Rev ID in the Save Dialog

PR 9070763: assembly relationships failing when modifying an assembly with center-plane relationships

PR 9125406: Placing a .asm that includes a .psm, shows wrong weld length

 

===Draft===

PR 9017656: Excel Table will not be correctly embedded as Picture

PR 9092148: File does not print after uncheck "Print to File" workflow

PR 9115998: Broken view changes on view update

PR 9128818: hatching on the cross-section wrong after updating the view 

PR 9129041: Extracting weld symbol information from an assembly does not work

PR 9123354: text scaling not correct during import

PR 9133649: Polylines are imported from DXF as bounded filled area, not only lines

PR 9002405: AutoCAD 2018 DWG support needed in Solid Edge

PR 9114494: Callout reference text size decreased each time when you do Update

PR 9012159: Hatch disappears in section view 

 

===Part/Sheet Metal===

PR 9160316: Solid Edge crashes when editing the color of the wire.

PR 9101065: Improved UI performance while deleting variables in the variable table

 

===Translators===

PR 8977646: Impossible to open Step file with ST10

PR 9124045: Import ACAD nested block has the wrong origin

PR 9091716: Partially DWG import incorrect, the hatch is missing 

 

===Illustrations & 3D Publisher ===

PR 9142477: Lost Save QSM button in SE after installation of MP06 for Technical publication

 

===Design Manager===

PR 9095978: Revision ID is not getting incremented properly for linked draft files

 

===Teamcenter Integration for Solid Edge===

PR 9153552: SaveAs fails to create Teamcenter objects having required properties

PR 9002242: Auto-assign is not working with smart codes

PR 9157460: File Properties dialog is shown as blank for FOA member

PR 9165641: Can't login from RAC PL and Solid Edge PL on the same user at the same time

PR 9168646: Problem with selecting items on SESE Parts List View by Ctrl+A

PR 9165958: Previously cleared values are added after Where Used

PR 9127806: Backport Feature - Honor new preference to clear properties

Regards,
Fred White
Siemens PLM Software
9 REPLIES 9

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Pioneer
Pioneer

Not sure where else to post this, but specifically since updating to MP8, the office has been having issues with Assemblies.

 

Specifically, when saving an assembly, the loading icon doesn't dissapear (ie doesnt save), and Solid Edge crashes.

 

Apologies if there's a bugs/glitches post somewhere, unaware of where that is if so.

 

We've had to uninstall the Maintenance Pack.

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@User_Error please contact your Solid Edge support resource so we can get this investigated for you.  

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Good morning/afternoon everyone,

 

Please see the screenshot below. In MP8 I don't see any update for the Teamcenter Integration as in MP1. Is it safe to say that no Teamcenter update is required for MP8?

 

Capture.JPG

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@TheodoreTurner  I believe that since the SEEC client is now part of the Solid Edge install, it is patched with the Solid Edge MP.  The download you are referring to appears to be for the SEEC Administrator tool only.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Hello @KennyG,

 

Thank you for the reply. Yes, I am referring to the SEEC Administrator tool. With some of the previous MP's there were new "feature_seec" XML files to update the "Teamcenter Integration for Solid Edge" template in the Teamcenter Environment Manager. I just want to make 100% sure MP8 doesn't also require a template update.

 

Capture.JPG

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

No, no template update required with MP8.  We now only post SEEC Administrator maintenance packs when there is a need for a template update.

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Thank you @uk_dave,

 

That's great news...this will save me a lot of time when installing new MP's.

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Siemens Genius Siemens Genius
Siemens Genius

Hi, 

 

the link http://support.industrysoftware.automation.siemens.com/general/email.shtml is broken, is there a new one to receive email notifications about launch of Maintencance Packs?

 

Thanks, 
Susann


Community Manager, Solid Edge
Teilnahmebedingungen | Jetzt Gast-Author werden!

Jetzt eine Solid Edge Zertifizierung erhalten!

Re: Solid Edge ST10 - Maintenance Pack 8 Announcement

Siemens Legend Siemens Legend
Siemens Legend

Hi Susann,

 

This will get you to the Email Subscription page:

 

https://www.plm.automation.siemens.com/global/en/support/email-subscription.html

 

 

Regards,
Fred White
Siemens PLM Software