Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST10 Simulation

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Can I simulate imported assemblies data (.step, parasolid ...) in Solid Edge ST10 Simulation ?

Thanks in advance for the answers!

5 REPLIES

Re: Solid Edge ST10 Simulation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes.  Once imported it becomes native Solid Edge data.  Just insure that when it imports, the surfaces stitch into solids.  Depending on the translator, I typically use the "Heal and Stitch" option.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST10 Simulation

Phenom
Phenom

Yea you can, though you'll have to convert it to Solid Edge data and build the FEA connections up as you would normally. 

 

Once it is converted to SE bodies you will be able to mesh them as if they were created nativly, plus if you use Syncronous, you can modify them easily to iterate the design-analyse-redesign-reanalyse.... process.

Re: Solid Edge ST10 Simulation

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I have ship structure with many parts. I can not set connectors automatically. So I thought that the problem may be of the imported geometry.

 

Thank you!

Re: Solid Edge ST10 Simulation

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thank you very much!

Re: Solid Edge ST10 Simulation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Don't forget about Geometry Inspector on the Inspect tab. It can help identify suspect geometry.

LMGi
www.TLMGi.com