Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Solid Edge ST10 Trial Download

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @uk_dave

 

 

 

Yes this is exactly I have seen here too.

 

There is more than enough space on disc, user is logged in as admin and starts the exe with RMB "Run as Administrator"

All rights for the folders are set completeley, 

 

What we can see was the error as last line in SE....log under %temp% 

 

can't create folder c:\SEWEBInstall\Solid Edge

 

I also have created this folder manually and restarted the exe as admin.

 

As mentioned by @Dariusz_IE  there maximal is a short blink and this was it.

 

 

regards
Wolfgang

Re: Solid Edge ST10 Trial Download

Creator
Creator

I did exactly the same - created Solid Edge folder manually but it didn't help, all the procedures described by @hawcad has been performed and still the same result.

Re: Solid Edge ST10 Trial Download

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @uk_dave

 

 

 

what I can see here, is, that both of us have Win7 computers.

 

Maybe this could be a hint?

 

 

regards
Wolfgang

Re: Solid Edge ST10 Trial Download

Siemens Phenom Siemens Phenom
Siemens Phenom

Download and install 7-Zip:

 

http://www.7-zip.org/download.html

 

Once you have 7-Zip, browse into the C:\SEWebInstall folder.

 

On the first 7z file, "Solid_Edge_Web_Package_ST10.7z.001", open this in 7-Zip.

 

You should then be see the Solid Edge folder and manually extract this folder to the disk:

 

2018-01-18 13_39_42-C__SEWebInstall_Solid_Edge_Web_Package_ST10.7z.001_.png

 

If you do not see the Solid Edge folder in this .001 file then one or all of your .7z files is corrupted.

Re: Solid Edge ST10 Trial Download

Siemens Phenom Siemens Phenom
Siemens Phenom

My screenshot showing my manually extracting the Solid Edge files from the download location is performed on a Windows 7 machine.

Re: Solid Edge ST10 Trial Download

Siemens Phenom Siemens Phenom
Siemens Phenom

You should have the following files with the following sizes:

2018-01-18 13_43_58-C__SEWebInstall.png

Re: Solid Edge ST10 Trial Download

Creator
Creator

I'm donwloading them again. I couldn't get the Solid Edge folder in 7ZIP. Watch this space...

Re: Solid Edge ST10 Trial Download

Creator
Creator

image.png

Re: Solid Edge ST10 Trial Download

Creator
Creator

@uk_dave as you can see, the last file is bigger than yours. And below is the screenshot from the 7ZIP.

There is no folder just another 7z file which can't be open by 7zip anymore.

 

image.png

Re: Solid Edge ST10 Trial Download

Siemens Phenom Siemens Phenom
Siemens Phenom

@Dariusz_IE just sent you a PM