Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST10 is Released!!

Community Manager Community Manager
Community Manager

All,

 

It is with great pleasure that I announce the release of Solid Edge ST10!! 

 

Solid Edge ST10 (110.00.00.107) will be available for download from https://download.industrysoftware.automation.siemens.com/download.php later this week once customer license files are available.  

 

ST10 is the first Solid Edge multilingual release – it includes all 14 languages.!

 

The process to upgrade subscription customers is underway. This upgrade and the 45-day trial download should be updated to ST10 by mid-August.

 

Solid Edge ST10 is download-only. DVDs can be requested by emailing dsom.plm@siemens.com, including the customer install number in the email text and “Solid Edge V110” as the email subject.

 

Enjoy!!

Laura

51 REPLIES 51

Re: Solid Edge ST10 is Released!!

Valued Contributor
Valued Contributor

Hi Laura Watson
I was waiting for this news.
I think it will be available from the beginning of next week because it is vacation period from this weekend.
Please be sure to release this week ... ^^

Re: Solid Edge ST10 is Released!!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

EXCELLENT!!!!! Love your work...keep it up "Team SE"!

 

ST10_Download.png

 

 

Just, sitting in the corner rocking back & forth, waiting to see the license file to become available......

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Solid Edge ST10 is Released!!

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

WoW! 14 languages at the same time. That's incredible and must have been a herculean task.

Congratulations to everyone involved in making this happen.

  

~Tushar

 

Re: Solid Edge ST10 is Released!!

Phenom
Phenom

Any information on multi-version install for ST10? I'd like to try it out alongside ST9 if this is still possible.

-Dylan Gondyke

Re: Solid Edge ST10 is Released!!

Siemens Phenom Siemens Phenom
Siemens Phenom

Same as with ST9.  Install the older version first, then install the newest version using silent install, and once both installed use the utility to switch between the active Solid Edge version.  See the readme file for complete details.

Re: Solid Edge ST10 is Released!!

Phenom
Phenom

Thanks!

-Dylan Gondyke

Re: Solid Edge ST10 is Released!!

Pioneer
Pioneer

Hi Laura,

 

Thanks for this update re ST10 availability.

 

We were getting concerned re having it on time to get our labs ready for the new academic year.

 

Is it right that the ST9 licence file will not work with ST10?

 

Regards,

 

Desmond Brown 

Ulster University

Re: Solid Edge ST10 is Released!!

Siemens Phenom Siemens Phenom
Siemens Phenom

Correct!  ST9 license files will *not* work with ST10 -- you will need a new ST10 license file.

Re: Solid Edge ST10 is Released!!

Valued Contributor
Valued Contributor

I was glad to come to the download server faster than I thought.
But .. License file is still for V109 only.
When will the Korean license file come up? ..