Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST10 on a USB Stick

Genius
Genius

Is it possible to get Solid Edge ST10 on a USB Stick instead of CD? 

I haven`t used CD/DVD drives for years.

Now, I must download the program from Gtac.

 

Best regards,

Geir

 

 

Solid Edge 2019
3 REPLIES 3

Re: Solid Edge ST10 on a USB Stick

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Create an ISO-Image and make use of Virtual DVD. That's the way we work.

 

Extremely flexible and fast

 

Stefan

smitsch@unitec.de
www.all4edge.de

Betreff: Solid Edge ST10 on a USB Stick

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

download and save onto a USB stick?

 

This is what I do for a couple of years and it works better than any DVD (faster).

And I have all DVDs available on the same USB stick.

A 16 or 32 GB is enough.

 

And as far as I remember there was an announcement with ST9, that this is the last vesion which will be released on DVD?

 

regards
Wolfgang

Re: Solid Edge ST10 on a USB Stick

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In my experience you can download directly to a thumb drive and install from it. No need for an iso image.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200