Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST10 save drawing as PDF fails

Legend
Legend

Hi,

 

When I try to save a drawing as PDF I get this error.

 

Error.jpg

 

Any idea what could be wrong..

 

I use Adobe acrobat 9.0   and PDFCreator also on this PC.

 

Kind Regards,

 

Jan Bos

Emmen, The Netherlands

3 REPLIES

Re: Solid Edge ST10 save drawing as PDF fails

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Check your Options on the Save As form and see if you have a sheet range specified by default under Sheet Options.  If a range is set and it is beyond the actual number of sheets contained in the drawing, it will fail.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Solid Edge ST10 save drawing as PDF fails

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Check if in your Devices and Printers have a Solid Edge Velocity PS Printer 2.0, if don't have printer with this name, you will need to install Solid Edge Printer. Go to Solid Edge folder install, Program folder, search about PrinterInstaller.exe, with closed Solid Edge, execute that and them verify if printer is there and test if you can save pdf.

Re: Solid Edge ST10 save drawing as PDF fails

Legend
Legend
I remember that I have cleaned out all those printers... and removed also the Solid Edge Printer.. not realising that it was used to create the pdf files..
Will have a look in the morning.. and report back..
Thanks so far

Jan