Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST4 Not responding in assembly.

N/A

Solid Edge ST4 Not responding when assemble drawing made in student addition version.

my computer specification below,
Acer 5738 Laptop
Intel Core 2 Duo 2.0 GHz
3GB DDR3 RAM
WINDOWS 7 ULTIMATE 32 BIT Operating System.

3 REPLIES

Re: Solid Edge ST4 Not responding in assembly.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
What environment are you in... Assembly or Draft? Sounds like you are trying to create a drawing of an assembly???


Ken

Production: ST10 MP6
Testing: SE 2019

Re: Solid Edge ST4 Not responding in assembly.

N/A
i am create drawing in assembly but when i am insert second part program not responding.

Re: Solid Edge ST4 Not responding in assembly.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
When you insert the second part, it is waiting on you to select faces to constrain the parts. Watch the bottom of your screen for the input it is expecting from you.


Ken

Production: ST10 MP6
Testing: SE 2019