Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST5 - Maintenance Pack 10 Announcement

Siemens Legend Siemens Legend
Siemens Legend

December 16, 2013

 

 

Dear Solid Edge Customer:

 

The latest Maintenance Pack (MP10) for Solid Edge ST5 is now available for download. Thanks for helping us make Solid Edge more productive.

  

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

  -- Windows 8 --

 

   Solid Edge ST6 will be the first release to support Windows 8.

  

   Solid Edge ST5 does not support Windows 8.  Any ST5 issues that are specific to

   Windows 8 or IE 10 cannot be addressed until ST6.  

  

   Based on our testing, most Solid Edge operations (Part, Sheet Metal, Assembly

   and Draft) work the same as on Windows 7 and Windows 8.  On Windows 8, we

   highly recommend installing Solid Edge ST5 to a non-default location (somewhere

   other than the default Program Files folder). 

  

   In some cases, .NET 3.5 had to be manually activated to use Solid Edge Tutorials,

   Insight, and Simulation Express.

  

   Solid Edge License Utility, License Borrowing, Embedded Client, Insight XT, Web

   Publisher, and Engineering Reference have known problems on Windows 8 and

   will not work successfully with ST5.

 

  -- Maintenance Pack Policy --

 

   We release Maintenance Packs for CRITICAL items only. Maintenance Packs are

   available up to a maximum of 15 months following the release date of the English

   version. The release date for Solid Edge ST5 English was 7/20/12, making the

   Maintenance Pack cutoff date 10/20/13.

 

================

Download Location:

================

 

ST5 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST5/ 

 

==========

Installation:

==========

 

After downloading the Maintenance Pack to your machine, unbundle the zip file and then

dbl click on exe to install the Maintenance Pack.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtmlfor the web interface.

 

Or send an e-mail message (message and subject line should be blank) to: sfbmail-subscribe.plm@siemens.com

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 6952126:  Replace all on alternate components from automation fails to replace all

PR 6931965:  Query on HolePtr.GetHoleData() raises exception with Synchronous mode ThreadHole

PR 6941513:  AssemblyChangeEvents constants having same enum number

PR 6945352:  Abort at JAsmMultiPartFeature:Smiley FrustratedyncPart when opening this assembly

PR 6935212: Added GetMatrix API to Sketch and Profile

PR 6941052:  a crash when calling CopySurfacePtr->GetName() API

PR 6940547: Crash on calling OrderedGeometry API present on Sketch Profile in Part Document

 

===Assembly===

PR 2224165: Fixes for crashes reported by customer via auto-crashlog capture

PR 2225795: Solid Edge does not allow changing material of Part if part file is modified outside

PR 6952137: Replace Part command resulting in incorrect display/locate/highlight while in-place active in a subassembly

PR 6936068: Solid Edge crashes when highlighting in a section view

PR 6941513: Event notification was needed when an occurrence was renamed

PR 1962190: Unable to 'transform to sheet metal' a thicken body created from copied surfaces

PR 6963231: Solid Edge shuts down when you Save As

PR 1963509: Problem when modifying with ST5 piping route made in ST3

 

===Draft===

PR 1957529: Etches are seen as assembly features

PR 1957933: Selecting callout saved setting after smart select results in crash

PR 6950735: Balloon are moved when we make the leader visible

PR 2225580: Text font export to DWG appears differently from ST5 than ST3

PR 6578739: Abort on SE close if draft document has link to an in-place activated subassembly

PR 6957060: Shading does not update correctly in ST6, MP2

 

===Part/Profile/Sheet Metal===

PR 1955449: pattern of parts on synchronous holes is wrong

PR 1959828: Crash when editing a line

PR 2224865: Problems creating and using profile elements more than 500m from origin

PR 6952582: Resolved case of invalid memory access

PR 6954471: Unable to open a part file

PR 1953392: Unable to Thicken from Part Copy

 

===Insight===

PR 1933721: "Free Text" search problem with option "Search for results in subfolders"

PR 1960321: Free text search shows only 50 hits even though more exists

PR 6840744: Where Used does not find DFT file

PR 6880776: Insight: FOP members are not listed as linked files in the LCA process

PR 6935532: Insight: Materials list is not available in Property Manager

PR 6963116: Open in Editor from Search WebPart gives a download message

 

===Insight XT Server, Standalone Client, Solid Edge Client===

PR 6940204: Add 2 SESP Unacceptably slow during dry run

PR 6943605: Add 2 SESP fails by writing invalid GUIDs, causing numerous other failures in SE

PR 6957972: Performance issues when Property Synchronize preferences = FALSE

PR 1952968: Slow memory growth/leak on multiple open close operations

 

===Solid Edge Embedded Client===

PR 1955168: Not able to Revise Item Revisions with MS Office Datasets

PR 6874493: Opening a large assembly is not honoring File Open settings

PR 6896782: SEEC: Enter key does not perform search

PR 6961653: Assign Item ID does nothing in the CPd after upgrading from ST4

PR 6938073: Crash changing Revision Rule in current opened assembly

 

Regards,
Fred White
Siemens PLM Software