Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST5 - Maintenance Pack 11 Announcement

Siemens Legend Siemens Legend
Siemens Legend

April 28, 2013

 

 

Dear Solid Edge Customer:

 

The latest Maintenance Pack (MP11) for Solid Edge ST5 is now available for download. Thanks for helping us make Solid Edge more productive.

 

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

  -- Windows 8 --

 

   Solid Edge ST6 will be the first release to support Windows 8.

  

   Solid Edge ST5 does not support Windows 8.  Any ST5 issues that are specific to

   Windows 8 or IE 10 cannot be addressed until ST6.  

  

   Based on our testing, most Solid Edge operations (Part, Sheet Metal, Assembly

   and Draft) work the same as on Windows 7 and Windows 8.  On Windows 8, we

   highly recommend installing Solid Edge ST5 to a non-default location (somewhere

   other than the default Program Files folder). 

  

   In some cases, .NET 3.5 had to be manually activated to use Solid Edge Tutorials,

   Insight, and Simulation Express.

  

   Solid Edge License Utility, License Borrowing, Embedded Client, Insight XT, Web

   Publisher, and Engineering Reference have known problems on Windows 8 and

   will not work successfully with ST5.

 

  -- Maintenance Pack Policy --

 

   We release Maintenance Packs for CRITICAL items only. Maintenance Packs are

   available up to a maximum of 15 months following the release date of the English

   version. The release date for Solid Edge ST5 English was 7/20/12, making the

   Maintenance Pack cutoff date 10/20/13.

 

================

Download Location:

================

 

ST5 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST5/ 

 

==========

Installation:

==========

 

After downloading the Maintenance Pack to your machine, unbundle the zip file and then

dbl click on exe to install the Maintenance Pack.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtmlfor the web interface.

 

Or send an e-mail message (message and subject line should be blank) to: sfbmail-subscribe.plm@siemens.com

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 6988146: get_NumAttachedObjects() returning a positive number of attachments

PR 6988067: PropertyTableAttached Attribute gets duplicated on feature removal

PR 6974666: Crash calling API Sketchs::AddByPlane

PR 6987955: Issue related to PropertyTableAttached Attribute after CopySurface in SE

 

===Assembly===

PR 1964934: Select all occurrences did not work properly for sub-sub assembly.

PR 1973819: Bad Performance when deleting Asm features

PR 6981399: Issue replacing adjustable parts and parts being over-constrained

PR 1964973: When modifying piping route, the elbows come with a wrong orientation

PR 1973819: Bad Performance when deleting Asm features

PR 1979380: Parts are hidden after removing a part in a pattern of adjustable parts

 

===Draft===

PR 1968968: Solid Edge stops working - non reproducible

PR 2231479: If V15Draft is opened by ST4, the value of a size will change

PR 6981703: copy/pasting drawing views

PR 1976521: Callout text disappears

PR 6974447: Secondary units incorrect for Fit Hole/Shaft with tolerance dimension

PR 7105469: Unable to change element gap on feature control frame

 

===Part/Profile/Sheet Metal===

PR 1950721: Request to reopen issue - Etch identify with API on the flatten model

 

===Insight===

PR 6927845: Slow to open in Revision Manager when components have families of parts

PR 1950953: "Replace Part with Copy" copies also unselected parts when using Insight

PR 1957847: Search Server Express 2010 French: Where Used doesn't find all documents

PR 1958674: Insight can't open files with umlauts via the search result list

PR 1961457: Insight Performance Regression: First Open and First Search are very slow

PR 6970943: Slow Operation during the opening of larger assemblies

 

===Solid Edge Embedded Client===

PR 1938118: SEEC Save As automatically assigns new Item to same Project as original Item

PR 1961950: Cannot set default or select value for Boolean property upon initial creation

PR 1966270: Replace Sub-Asm with copy duplicate occurrences in TC structure manager

PR 2211862: SEEC "add to Teamcenter" failed when ST4 and TCX have attribute mapping

PR 2229264: Paste operation time increase dramatically with the BOM lines

PR 6931640: FMS error message is displayed on file open

PR 1915659: Unable to place more than one FOP member into an assembly without error

PR 6889752: Cached XML configuration files

PR 6901072: BOM mismatch error shown when saving this FOA

PR 6901822: SaveAS is linking source model to draft instead on the newly created model

PR 6963346: CheckOut of Embedded Client License does not show up in debug.log

PR 6754049: Dragging unmanaged part into managed draft gives error message 3 times

PR 6944040: Unable to drag text from unmanaged dft to managed dft

Regards,
Fred White
Siemens PLM Software