Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST5 on Windows 8

N/A

I am running Windows 8 on a boot camped Macbook Pro, I can download Solid Edge ST5 but whenever I go to install it I get the error message "This installation package could not be opened. Verify that the package exists and that you can access it, or contact the application vendor to verify that this is a valid Windows Installer package" can anyone offer a solution?

2 REPLIES

Re: Solid Edge ST5 on Windows 8

Esteemed Contributor
Esteemed Contributor
Wait till ST6 is available. ST5 does not support Windows 8.


Ken

Production: ST10 MP5
Testing: SE 2019

Re: Solid Edge ST5 on Windows 8

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Ken is right in that ST5 does not support Windows 8, but from the readme you will find that it can be installed and that it is running under Windows 8 with only a few exceptions. Siemens just does not support any problems of ST5 under Windows 8.
But your problem, does not seem to be that. It seems that your package is broken and you might try to download it again with a download manager.