Solid Edge ST5 when working on large assembly, and open a drawing to print it out..Puffff crashes SE

Valued Contributor
Valued Contributor

Can any one help me with this ...

it is pretty annoying when ever it is crashing 

MfG -
Viv
2 REPLIES

Lots of reasons this is happening.  First thing comes to...

Esteemed Contributor
Esteemed Contributor

Lots of reasons this is happening.  First thing comes to mind is memory or a lack of... What are you running for OS (include bit version), physical memory and bit version of SE?

 

SE typically exports a Crashlogf.txt file located in C:\Users\yourusername\AppData\Local\Temp.  Contact your VAR or GTAC directly if able and provide them the file and the steps you are doing that results in a crash and they can typically pinpoint the issue.

 


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Lots of reasons this is happening.  First thing comes to...

Valued Contributor
Valued Contributor
Grundey ! U r right ... ! It was lack of ** but i m running on 64 bit Version ... Thank U for Ur answer !
MfG -
Viv