Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST6 - Maintenance Pack 13 Announcement

Siemens Legend Siemens Legend
Siemens Legend

February 13, 2015

 

 

Dear Solid Edge Customer:

 

The latest Maintenance Pack (MP13) for Solid Edge ST6 is now available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

--- Office 97-2003 File Types ---

 

Customers have reported problems with SEEC interacting with Office 97-2003 file types.

 

   Example: It not possible to open an excel spreadsheet from the Solid Edge variable table.

 

File open is failing because Microsoft Office 2010 added security checks relating to

opening Office 97-2003 files. Therefore, in order to open Office 97-2003 file types 

in this manner the SEEC Cache folder location must be added to the Microsoft Office

application’s Trusted Locations.

 

   Example: Add the SEEC Cache location to:

 

      File->Options->Trust Center->Trusted center settings->Trusted locations

 

================

Download Location:

================

 

ST6 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST6/ 

 

==========

Installation:

==========

 

After downloading the Maintenance Pack to your machine, unbundle the zip file and then

dbl click on exe to install the Maintenance Pack.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

Or send an e-mail message (message and subject line should be blank) to: sfbmail-subscribe.plm@siemens.com

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===Assembly===

PR 7250477: Show Only command does not work on a part in a large assembly

PR 7286828: modification during IPA is dismissed if you cancel the delete/suppress-dialog in assembly

 

===Draft===

PR 1937906: Text within a block with orientation Center Left exported with wrong position

PR 1989981: SE ignores the defined Font Mapping on export of Textboxes as MTEXT

PR 7272043: In Text box properties "Justification" value is not correct. Please fix in ST6

PR 7223230: Some text not searchable when saved out to PDF

PR 2247261: parallel dimensions in ST3 when opens in ST6 the dimension positions are changed

PR 2249099: Dimensions move when you open the provided daft in ST6

PR 2249101: Moving one dimension causes placement change in another

PR 7276910: Grid-Origin moves after switching sheets

 

===Insight===

PR 7207681: Non-string properties are deleted from files

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7195427: Opening file with custom status of 31-Locked displays incorrectly in Read Only

 

===Solid Edge Embedded Client===

PR 7263188: Property not updated in draft because reverse property sync of children skipped

PR 8250584: Localized ATTI unable to successfully validate and upload files

PR 8252712: Add to Teamcenter crashes when uploading assembly

PR 7169854: Item Name in Solid Edge CPD not synchronizing between Part and Draft file

PR 7219661: Density for selected Material on SEEC CPD does not match SE Material.mtl

PR 7278961: CFG file is not being uploaded to TC for an assembly having no links or component

PR 7278977: Draft image files such as emf, jpg, bmp etc. are not carried forward during Revise

PR 7250239: Mandatory attribute not being set during Solid Edge Draft save

PR 7251662: Bad performance in new SEEC implementation.

 

 

Regards,
Fred White
Siemens PLM Software