Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST6 - Maintenance Pack 14 Announcement

Siemens Legend Siemens Legend
Siemens Legend

April 28, 2015

 

 

Dear Solid Edge Customer:

 

The latest Maintenance Pack (MP14) for Solid Edge ST6 is now available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

--- Office 97-2003 File Types ---

 

Customers have reported problems with SEEC interacting with Office 97-2003 file types.

 

   Example: It not possible to open an excel spreadsheet from the Solid Edge variable table.

 

File open is failing because Microsoft Office 2010 added security checks relating to

opening Office 97-2003 files. Therefore, in order to open Office 97-2003 file types 

in this manner the SEEC Cache folder location must be added to the Microsoft Office

application’s Trusted Locations.

 

   Example: Add the SEEC Cache location to:

 

      File->Options->Trust Center->Trusted center settings->Trusted locations

 

================

Download Location:

================

 

ST6 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST6/ 

 

==========

Installation:

==========

 

After downloading the Maintenance Pack to your machine, unbundle the zip file and then

dbl click on exe to install the Maintenance Pack.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

Or send an e-mail message (message and subject line should be blank) to: sfbmail-subscribe.plm@siemens.com

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 8252701: Assembly Relations are lost when using "TranslateMultipleOccurrences"

PR 7325992: SetPropertiesInfo API does not allow the dataset name column to be cleared

PR 1996278: Unable to access edgebar features via API

 

===Assembly===

PR 1993287: Occ prop dialog shows wrong rotation values

PR 7295498: Parts jump on update all

PR 1992274: Changes made with Physical Properties not handled correctly

PR 7286889: physical properties calculation saves material to part

PR 7288288: Handle points of frames moved after Update all links done

PR 7217433: Assembly constraints become corrupt when using MultiCAD driven references

PR 7329238: Files opening with Read Only status when they are available

PR 8700613: Part copy needs update without model's change

 

===Draft===

PR 1991000: When saving to Dwg, 'Solid Edge ISO' textfont is not converted to textfont 'Aria

PR 2250493: abort when un-breaking views in some cases

PR 7212177: a drawing view did not depict correct assembly feature in some cases

PR 7216837: In ST6, the text "jumps" to a higher position in the callout box

PR 7300949: Wrong dimension value for tangent dimension

PR 8261329: crash while using a new configuration file for a specific draft to dxf export

PR 7288091: DV become out of date, once an assembly has been opened

PR 7335228: Opening a DFT file crashes Solid Edge

 

===Part/Profile/Sheet Metal===

PR 7149122: Incorrect scaling applied for Part Copy if value is not followed by Enter or Tab.

PR 7234789: Expression in Variable table fails during attempt on Sync edit

 

===Insight===

PR 8261192: Insight Search lists all documents twice after an upgrade from V20 (WSS2) to ST7

PR 7332037: Getting a “Cannot download a document" message

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7285591: IE10 - Crash seen on sending any SESP objects to Relation Browser

 

===Solid Edge Embedded Client===

PR 6997635: Save As on Solid Edge Draft in SEEC gives incorrect filename

PR 7271453: ATTI French consistently crashing

PR 7305483: Solid Edge Model file remains checked out to me while the Draft is checked in

PR 8254839: Localized AddToTeamcenter Interactive unable to display property columns for certain dataset

PR 8263114: AddToTeamcenter interactive doesn't honor the preference SEEC_property_item_name

PR 7332854: does not assign project info, correctly during a revise operation

PR 7334006: Local BOM Precision Override

PR 7324478: Save As copies ItemRevision name from source to new object in 10.1.3

PR 7341209: Item Numbers in SE Assembly are not synchronized with Find Numbers in TC

PR 7355760: Revise generates Partial Error

PR 7283519: ASM occurrence property, Item Number are not being maintained from the TC BOM

 

Regards,
Fred White
Siemens PLM Software