Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST6 Maintneance Pack 3 was Released 11-25-2013

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

I haven't seen a post on this site yet, so I thought I would mention it.

 

Solid Edge ST6 Maintneance Pack 3 was Released 11-25-2013.

 

As usual, you should find Solid Edge ST6 files at:

https://download.industrysoftware.automation.siemens.com/solid_edge/ST6/

5 REPLIES

Re: Solid Edge ST6 Maintneance Pack 3 was Released 11-25-2013

Pioneer
Pioneer

Hi,

Have tried the link, but how do you actually get to the download part, as to be honest

it all seems a bit of a maze to find it,

 

 

Re: Solid Edge ST6 Maintneance Pack 3 was Released 11-25-2013

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Ptr2 wrote:

Hi,

Have tried the link, but how do you actually get to the download part, as to be honest

it all seems a bit of a maze to find it,

 

 


Hi there,

 

The link @jinglis provided takes you [once logged in] directly to the ST6 section of the download directory....so click on, Solid Edge > choose either 32bit or 64bit [relative to the SE install, not OS] > MP03 [or any other available]....and it should start downloading.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Solid Edge ST6 Maintneance Pack 3 was Released 11-25-2013

Pioneer
Pioneer

Thanks Sean all done,

 

 

Re: Solid Edge ST6 Maintneance Pack 3 was Released 11-25-2013

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Most welcome.  Robot Happy

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Solid Edge ST6 Maintneance Pack 3 was Released 11-25-2013

Experimenter
Experimenter

FYI - If you use SEEC and Structure Editor, test ST6 MP3 fully. We found issues and had to abort our upgrade last Friday.