Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST6- Save as a .pdf

Experimenter
Experimenter

How do you save a cad drawing as a .pdf in Solid Edge ST6 2D CAD? When clicking on save as and looking at the possible types of documents to save it as I don't see .pdf. Is there something else I have to do? I need this .pdf for a milling machine.

1 REPLY

Re: Solid Edge ST6- Save as a .pdf

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

You may as well try posting this in the Solid Edge 2D Drafting Forum.

From the Solid Edge Application button, select Save As - Save As Translated, then PDF from the list. This is just a guess, so not sure if the PDF option is available in the list:

 

sepdf1.png

 

sepdf2.png