Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST6 What's New

Experimenter
Experimenter

Need Help

 

I am a car carrier designer. How can I profile vehicles using solid edge to fit my models?  Thanks in advance.

3 REPLIES

Re: Solid Edge ST6 What's New

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

I would use a background image of a vehicle manufacturers spec sheet [like that attached], and trace over it using sketch tools......how do you want to use/show this? [are you just exploring it in the 3D model, of displaying it for dimensioned draft sheets, or even setting up renders?]

 

holden-commodore-2006.gif

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Solid Edge ST6 What's New

Experimenter
Experimenter

Hi Sean

 

My problem is I can not paste to  part protrusion.  What did I do wrong?

Re: Solid Edge ST6 What's New

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

I have ST8, so can't provide an example file that you can open natively with ST6, but basically the steps are...

 

  1. Open new part file [if wanting to use sketches only in ASM, then use create-in-place to start....]
  2. Create sketch on suitable plane, place image, position and scale as required, trace over image capturing relevant geometry [I normally place image on it's own sketch, then new sketch for tracing....so I can show/hide the image during tracing]
  3. Extrude desired regions of traced sketch if solid model is needed, or just leave as sketch[s].

 

Hope that's what your looking for.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019